Part Number: TPS62873 Tool/software: Hi team,
My customer has the concern about the output voltage change when changing the value of VRANGE bit. My customer just wants to change the output voltage steps, but it seems the output voltage range also changes…
Part Number: TPS62873-Q1 Tool/software: Hi Team,
A quick question, when TPS62873-Q1 power off, is there any internal path for power down? What is the power off slew rate or resistance?
Thanks
Best,
Frank
Part Number: TPS62873 Other Parts Discussed in Thread: TPSM8287A12 Hi,
Is there any functional difference (except temp. range) between TPS62873 Z0 and TPS62873 Y1Q ?
Both would be used with 6.2k to GND for VSEL (0.8V) and FSEL (2.25MHz)
Thanks
Part Number: TPS62873 Tool/software: Hi all, I have tested TPS62873 start up and shut down time. I found out there is a huge different between these two. Can someone explain why this would happen?
It takes 784us to start up the device…
Part Number: TPS62873-Q1
Tool/software:
I'm currently simulating the AC loop response using the provided model . My schematic is configured with VIN = 5V, VOUT = 2V, and FSW = 2.5MHz. However, my plot shows the trace of DB(V(VOUT)) with the y-axis…
Part Number: TPS62873-Q1 Other Parts Discussed in Thread: TPS62873 Tool/software: Hi TI,
I want to know how to select compensation R,C of TPS62873Y1.
These are Ti's Guide about comp R, C
AP EVM
PWR EVM
Datasheet
Rz
1.8k Ohm
2.43k Ohm
2.4k…
Part Number: TPS62873 Tool/software: what’s difference between TPS62873QWRXSRQ1(automotive) and TPS62873Z1WRXSR(common part)? these two parts shows same ratings from TI electrical characteristics datasheet.
Part Number: TPS62873-Q1 Tool/software: Hi,
How to choose peak-to-peak inductor current ripple if I have more than working condition which have quite different output current like 1A and 10A?