Part Number: AWRL6432 Other Parts Discussed in Thread: TPS62902-Q1 , , TPS628502-Q1 Tool/software: Hi,
May I have your feedbacks regarding to use TPS62902-Q1 to company with AWRL6432? https://www.ti.com/lit/ds/symlink/tps62902-q1.pdf
Customer want…
Part Number: TPS62902-Q1 Other Parts Discussed in Thread: TPS62902 Tool/software: Hello,
In our project, we are using TPS62902 to supply 1V25 Core supply.
Schematic is attached
We want to optimize BOM and reduce the reel amount for the pick and…
Part Number: TPS62902-Q1
Tool/software:
Hi,
Greetings of the Day !!
I could not find the Switching frequency limits other than the typical value of 2.5MHz.
It would really mean a lot if you can please help to get the frequency tolerance.
…
Part Number: TPS54225-Q1 Other Parts Discussed in Thread: TPS62902-Q1 , TPS54225 Hello, Looking for failure rate and failure modes information for the part number "TPS54225TPWPRQ1".
Thanks
Hi Zachary,
As Tahar mentioned TPS6287x-Q1 family can be used if 6.1A is required at the output. The 6.1A looks to be the max current that can be drawn and depending on the XPE, if you confirm a 1.112A draw then a lower current device like TPS62902…
I would recommend the newest TPS62902-Q1 which is about to release in a week or two on ti.com. For now, you can refer to TPS62903-Q1 datasheet which is already released. Performance on efficiency/frequency is identical on both devices. TPS62902-Q1 is…
Part Number: TPS62901 Other Parts Discussed in Thread: TPS62902 , TPS62903 , TPS629203-Q1 , TPS65131-Q1 Tool/software: Hello. I need to know the power dissipation of the following components:
TPS62901
TPS62902
TPS62903
TPS629203-Q1
TPS65131…
Part Number: LMR33630-Q1 Other Parts Discussed in Thread: LMR33630 , TPS62902 Hi team,
I want to find a device, Vin from 5.1V to 12V, Vout =5V, Io from 0.5A to 1.5A. It seems that when the Vin is 5.1V, the LMR33630 Vout can't supply 5V. Do you have…
Other Parts Discussed in Thread: TPS629210-Q1 , TPS629210 , TPS62902 , TPS62140 , TPS54320 , TPS54326 How are new designs being supported with the current supply chain issues?
All the parts that were available at the start of design were available…