Hi Peter,
I also forget to mention that there is sub 1 A family of the above devices that you can consider as well. TPS629210, TPS629206, and TPS629203. they can do a low as 300mA and very good efficiency at light load with DCM mode
https://www.ti.com…
Part Number: TPS62110 Other Parts Discussed in Thread: TPS629203 Hi Can you share the calculations for TPS62110MRSAREP
VIN=10V(4-20mA)
VOUT=3.3V
IOUT=0.01A(Only 6mA required)
FSW=1MHz
Can you share the calculation for both inductor input and output ca…
Hi Ross,
TPS62120 min current limit is 200mA. It cannot improve load current to 200mA. We don' t have any p2p replacement with >200mA output current for TPS62120. However, we do have the new generation Buck converter with 300mA. TPS629203 is 300mA load…
Part Number: TPS62125 Other Parts Discussed in Thread: TPS629206 , TPS629210 , TPS629203 , Hi,
The TPS62125 configured as inverting buck-boost application is very risky. We strongly recommend using our new generation buck converter TPS629203 or -Q1 family…
Part Number: TPS62120 Other Parts Discussed in Thread: TPS629206 , , TPS629210 , TPS629203 , TPS62122 Hi,
The TPS62120 or TPS62122 configured as inverting buck-boost application is very risky. We strongly recommend using our new generation buck converter…
Hi Pratik,
We don't have pin to pin compatible part with TPS62745. Are you open to different package? Please take a look our latest version of Buck converter TPS629203 in the link as below.
https://www.ti.com/product/TPS629203?keyMatch=TPS629203&tisearch…
Hi Thomas,
Understood.
Please look at TPS629203 (300mA max ), or TPS62903 devices (3A max).
You may also consider other TPS629XX products, just make sure those have the precise EN threshold and hysteresis feature.
Regards,
Yitzhak
Hi Amal,
There is not currently a pin-to-pin device with the same packaging for this part. However, a similar device that has Vin = 3-17V and programmable output voltage is TPS629203 .
Are there any specific design requirements for input/output voltage…
Hi Brian,
I would recommend newly released TPS629210/TPS629206/TPS629203 family with smaller size and super performance. For-5V application, please refer to application note in the link as below. The device and buck EVM are available now. You can easily…
Hi Matt,
TPS62125 is the old device. Now we have new generation buck converter TPS629210-Q1 (automotive) and TPS629210(Commercial). We have TPS629203(300mA) and TPS629206(600mA) parts as well. 1A part will be released by end of this year. The parts and…