Part Number: TPS629210-Q1 Hi Team,
I was looking for 12V to 5V conversion with around 1A current. If I would get schematics and PCB files, it will be easy for me to implement it in my design.
Thanks in advance.
Shubham
Part Number: TPS629210 Hi team,
Can this device output 0.5V? In case of external divider, Vout range is 0.6V to 5.5V. In case of internal divider, 0.4Vout and 0.6Vout are available.
Is it possible to output 0.5V by using a resiter which is between…
Part Number: TPS629210-Q1 Hi, I saw a similar forum regarding using in between values for the Rset value to get a certain voltage but had no clear answer. My question is are we able to use resistors inbetween the Rset to Voltage chart and get different…
Part Number: TPS629210-Q1 Dear TI experts,
My customer asked buck converter under the condition below.
Vin=5V
Vout=0.5V
Iout=1A
AEC-Q100 is required.
Actually I suggested TPS62921-Q1 based on WEBENCH simulation.
But it simulated as 0.4V…
Part Number: TPS629210 Tool/software: Hi Sir,
could you please help us review this layout? for U6, which is the TPS629210 sync buck converter power.
does our layout planning have any issue? thanks for your great support and learn from you.
(1…
Part Number: TPS629210-Q1 Tool/software: I would like to have some help with the Failure Mode Distribution for the following part number TPS629210-Q1 , this is usually included in the Functional Safety FIT Rate, FMD and Pin FMA report , but I cannot locate…
Part Number: TPS629210 Other Parts Discussed in Thread: TPS62160 Hello,
As a follow-up to one of my previous questions , where when I set the Vin component of the circuit to 5V in and set the parameters to 1.2V out at 100mA, this gave an output of 0V…
Part Number: TPS629210 Other Parts Discussed in Thread: TPS62160 Hello,
I am trying to simulate TPS629210 using WE Bench Simulator. The circuit I'm simulating has a 5V input voltage and requires a 1.2V output at 100mA. The circuit design can be found…
Part Number: TPS629210 Other Parts Discussed in Thread: TPS629206 I am looking for a small, highly efficient Buck Converter at light loads for a Microcontroller and some low current peripherals. Max current is around 500mA, but most of the time the microcontroller…
Part Number: TPS629210 Tool/software: Dear TI Engineer,
Is there any information about the minimum voltage difference between the input and output voltages of TPS629210? If the output is 3.3V, what is the minimum input voltage?
Thanks,
Kind…