Hi Sathishkumar V,
Please look at TPS629210-Q1 in the link as below.
https://www.ti.com/product/TPS629210-Q1?keyMatch=TPS629210-Q1&tisearch=search-everything&usecase=GPN
Thanks,
Nancy
Part Number: TPS62125 Other Parts Discussed in Thread: TPS629206 , TPS629210 , TPS629203 , Hi,
The TPS62125 configured as inverting buck-boost application is very risky. We strongly recommend using our new generation buck converter TPS629203 or -Q1 family…
Part Number: TPS62120 Other Parts Discussed in Thread: TPS629206 , , TPS629210 , TPS629203 , TPS62122 Hi,
The TPS62120 or TPS62122 configured as inverting buck-boost application is very risky. We strongly recommend using our new generation buck converter…
Hi Kygo,
TPS629120-Q1(automotive) or TPS629210(commercial) have pretty similar features with RP550L001B. TI parts have only one channel. But the efficiency is much higher at light load. TI parts have very small size with 1.6x2.1mm. You can use two with…
Other Parts Discussed in Thread: TPS629210 , TPS629210-Q1 Hello, Looking for smd voltage regulator
Input : 11 to 15 VDC Output : 5 VDC @ 0.6 A
We have limited PC board space.
Thanks,
Hi Gerald,
We don't have any PSPICE model for TPS62056. This is old converter. Are you open to use our new generation converter TPS629210-Q1 or TPS629210? TPS629210-Q1(automotive) was already released. The PSPICE model, EVM and parts are available now…
Hi Marcel,
Unfortunately, you could not adjust output voltage with external feedback resistor. Because the the real FB pin is inside device. If your output current is less than 1A, you may consider our latest buck converter TPS629210-Q1 with small size…
Hi Jay,
TPS62170 and TPS62125 are pin to pin compatible with TPS62162. Please check if TPS62170 and TPS62125 are available. I would recommend our new generation TPS629210-Q1(automotive) or TPS629210(commercial). TPS629210-Q1 will be released in Dec, 2021…
Hi AnBer,
No, we don't have a plan to have TPS629211-Q1 IND version. The only difference is Vin max between TPS629211-Q1(10Vin max) and TPS629210(17Vin max). You can use TPS629210 for IND application.
Thanks,
Nancy