Part Number: TPS62932 Tool/software: Hi TI Team,
I would like to ask a question.
Is the leakage current at the IFB terminal of the TPS62932 in the suction direction?
Part Number: TPS62932 Tool/software: Hi Team, We are using TPS62932DRLR, DC-DC Buck converter in our designs.We are looking for an isolated switcher or module, As this module is not supporting isolated Vout.
Please suggest an isolated part with the…
Part Number: TPS62932 Tool/software: Hi TI,
I experience exactly the same problem here. The device can run for hours without a problem. After cutting and reapplying power the device blows out sometimes. This happened to multiple machine produced boards…
Part Number: TPS62932 ① the switching frequency when I exit PFM mode is different from the set frequency. When the load is low even after exiting the PFM mode, does the set frequency sometimes not reach?
② the frequency setting is set to 2.2MHz, but…
Part Number: TPS62932 Other Parts Discussed in Thread: TPS62933F Tool/software: My customer is currently evaluating and would like to use TI's TPS62932 not to enter DCM mode. It was confirmed that DCM mode was entered at 500mA at 600kHz and 200mA at 1…
Part Number: TPS62932 Hi I designed board with TPS62932 and measured efficiency does not meet datasheet's efficiency. Schematic of tested board: Power supply connected to V_IN Programmable DC load connected to 3V3 The results: Datasheet efficiency: So…
Part Number: TPS62932 Hi team,
In the customer system, the actual load is about 0.5 A. They want to use a suitable inductor to reduce size.
However, there is a high current of 2A or more during OCP. They have to do a protective performance test and…
Part Number: TPS62932 Hi team,
Is there available max power data?
It is best if you have a graph that plots the output voltage or output power on the one axis with the output current on the other axis.
Customer assume that 5V × 3.5A = 17.5W. And…
Part Number: TPS62932 Other Parts Discussed in Thread: TPS62933F , TPS62933O
Tool/software:
Hello,
I'm validating the design and layout of a 20V to 12V buck converter using the TPS62932, and am observing some unexpected behavior on the voltage…
Part Number: TPS62932 Tool/software: Hi Team, we are using TPS62932DRLR regulator in our design. We have noticed that DCDC does not work properly in some cases, particularly once the power supply is given the DCDC starts to get hot and propably damaged…