Part Number: TPS62933 Hi Ti,
I am trying to use TPS62933 as inverter, input 12V, output -5V/3A, would you please help to review below circuit design is OK or not?
Part Number: TPS62933
Hi Ti,
I am trying to use TPS62933 as inverter, input 12V, output -5V/3A, would you please help to review below circuit design is OK or not?
Part Number: TPS62933 Hi TI Specialist:
I have some queries for TPS62933 converter during try to create a new simulation file for testing, but i couldn't find the key parameters from the datasheet on website, please help to check and advise, thanks…
Part Number: TPS62933 Other Parts Discussed in Thread: INA180 I am utilizing the INA180 for monitoring DCDC current. The INA180 amplifies the voltage across the current sensing resistor, presenting a sine wave pattern as observed on the oscilloscope. Consequently…
Part Number: TPS62933
Hello team,
My customer wants to use this device in condition below:
VIN: 24V
VOUT: 12V
IOUT: 0.5A
FSW: 500kHz
However, customer wants to use inductor of 10uH, which will result inductor ripple current to be 200% of IOUT. Datasheet…
Part Number: TPS62933 Hi, when TPS62933 has no load (Iout=0A), the SW signal has oscillations. Is this normal?
When there is a load (Iout>0A), the SW signal is nice clean PWM/square wave.
Part Number: TPS62933
We are making a cost-effective power distribution board for our drone.
The board is supposed to supply :
20A at 17.4V to a 4in1 ESC (powering 4 BLDC motors) max.
5V to flight controller at 3A max.
12V to video transmission…
Part Number: TPS62933 Other Parts Discussed in Thread: LM5148-Q1 Hi Team,
Could you possible help to check if we have similar device as below competitor? Customer requirement is input voltage 9V+, and output voltage is -32V, and output current is 2.4A…
Part Number: TPS62933 I designed a DC-DC circuit with TPS62933, input 18V, output 15V 2.5A, inductor=6.8uH, Fsw=500kHz. Cout>200uF.
when this circuit work with the load which is an Audio PA. the load is light when no music playing, then an audible noise…
Part Number: TPS62933
Hi, I'm using 16VDC Vin (good quality, enough input current) to power up my TPS62933 board. The nominal frequency is 2.2MHz. The Vout is stable when Iout<=2.6A. When Iout>2.6A, TPS62933 turns ON and OFF rapid ly. I follow…