Part Number: TPS62933P Other Parts Discussed in Thread: TPS62933 Hi,
During the product development, we found a condition where a short circuit of two adjacent pin results in potential fire.
When connection between BST and PG is shorted, the device…
Part Number: TPS62933P Hi,
While testing the device, voltage measured at switching terminal exceeds absolute maximum rating.
These only happen when switching terminal is transitioning from low to high. I would like to know if these over-voltage condition…
Part Number: TPS62933P Other Parts Discussed in Thread: TPS62933 , , TPS56837 , TPS62933EVM
Tool/software:
Hello TI,
input: 24Vdc
Out put 12Vdc/ 3A required
I have design the circuit with TPS62933PDRLR. But i am not able to use 1.2MHZ or 2.2Mhz…
Part Number: TPS62933P Other Parts Discussed in Thread: TPS54302 Hi,
I'm seeing unusual behavior while current probe is inserted at the output of DC-DC converter. Once I remove the probe, output waveform become normal. It is also not oscillating with…
Part Number: TPS62933P Other Parts Discussed in Thread: TPS62933F Hi TI team,
I have 2 questions regarding TPS62933P.
Below is my schematic. Fsw is 1200kHz, Vout is 1.5A.
The surrounding component are selected based on this recommended LC combination…
Part Number: TPS62933P Other Parts Discussed in Thread: TPS62933 Hi team,
I am currently designing the power circuit for Spartan-7 FPGA. According to the Xilinx Power Estimator, the power consumption for my application is less than 3 W. I have designed…
Part Number: TPS62933P Other Parts Discussed in Thread: LMR51440 , Hi team,
I want to find a buck that support below conditions. The background is that I want to use it to output -20V. And I can't find a suitable device in TI.com. The actual input voltage…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: TPS62933P I am trying to run a Monte-Carlo simulation for TPS62933P step down converter but getting the the error 'ERROR(ORPSIM-16551): Floating point computation failed during Device/Model Load…
Part Number: TPS62933F Other Parts Discussed in Thread: TPS62933P Dear expert,
my customer is using TPS62933F, but we find the input power supply will be short when power up. could you help to check the schematic. thanks.
BR
Chi