Part Number: TPS62A03 Tool/software: Hi, TI expert
The customer requested a schematic review using TPS62A03.
[spec]
- Input : 3.2Vdc ~ 4.15Vdc
- Output : 3Vdc , 3A
Are there any problems with the circuit? Are there any areas that need to…
Part Number: TPS62A03 Other Parts Discussed in Thread: TLV62585 Hi team,
What is the specific threshold current to enter PSM?
It would be best if there is the plot that fSW vs Iout like TLV62585 datasheet.
Best regards, Goto
Part Number: TPS62A03
Hi,
Do you have any data or graphs showing the characteristics of output voltage vs output current (load regulation)? If so, could you please provide them?
If possible, I would like data for the following conditions:
VIN…
Part Number: TPS62A03 Tool/software: Hi TI team,
Based on the datasheet, the θJA is 157.3. This data is very high for a power chip.
Can you confirm if there is any error in this data?
If the condition are:
Vin: 5V, Vout: 4.2V, Iout: 3A, efficiency…
Part Number: TPS62A03 Tool/software: Hello,
On the datasheet "6.5 Electrical Characteristics" under "ENABLE"
Are the values of the "EN high-level input voltage" and "EN low-level input voltage" in the incorrect "MIN" & "MAX" locations ?
Is the…
Part Number: TPS62A03 Tool/software: Hi Team, Can you please share FIT and MTBF data for TPS62A03DRLR? It is not available on our website. Thanks & Regards Kunal Dhawan
Part Number: TPS62A03 Tool/software: Hi team,
In the datasheet, 1uF or 0.47uF are recommended as output inductor. Is there any performance difference between these two value? Best regards, Goto
Part Number: TPS62A03 Tool/software: Hello,
I am using the TPS62A02DRL_TRANS PSICE - there is no PSPICE for the TPS62A03
My parameters are 3.8V Vin, 3.3V Vout at 0.3A load and I currently have a 200K resistor from the VIN to the EN pin
My question…
Part Number: TPS62A03 Tool/software: Dear Team
On page #5
There are 2 kinds of FB value, one is 1%, another one is 1.5%, could you please teach me what is the difference?
(I'm looking for 1% parts)
https://www.ti.com/lit/ds/symlink/tps62a03…
Part Number: TPS62A02A Other Parts Discussed in Thread: TPS62A03 Hi,
May I know the TPS62A03 RTM schedue?
As I know seems sample release on Jun?
Thanks!
Jeff