Part Number: TPS63000 Dear Sirs,
We want to replace competitor with our TPS63000.
However, their thermal pad is a little different.
Since they are p2p and customer no need to modify their layout but thermal pad.
Is there any problems if those 4 pads…
Part Number: TPS63000 Other Parts Discussed in Thread: TPS63050 Hi team,
Customer measured that tps63000 has big inrush current during startup that would pull Vin a little lower.
Startup test condition,
Input is 5V, output is 5.5V/no load, EN is enabled…
Part Number: TPS63000 Hello,
From datasheet, the TPS63000 output range is 1.2V~5.5V.
Currently I am setting its output = 1.2V with external resistor divider as below circuit.
As it's the min value of this regulator, I am sure any problem or not.
…
Part Number: TPS63000 Hi,
We have a few design where we are using " TPS63000IDRCRQ1" , " TPS63000" and "TPS630001" since last 2-3 years but we are facing consistent issue.
For the Developmental testing purpose when we try…
Part Number: TPS63000 Hi Experts,
Good day! This queries is about buck-boost converter, TPS63000.
Can you clarify us about the PS/SYNC pin? Is this for more of a stand by use? Or is it for using the part at lower currents?
Client has to use the TPS63000…
Part Number: TPS63000 Hello.
I use TPS63000 and have some questions.
Condition1. Current conspumtion is under 100mA.
Condition2. Input voltage is 5.0v and Output voltage is 3.3V .
Q1. There is high frequency sound, when I touch by hand on operation…
Part Number: TPS63000-Q1 Other Parts Discussed in Thread: TPS63000 Hi,
My TPS3000 buck/boost design does not work properly. The IC draws a lot of current from the input supply and gets very hot. The input voltage is unregulated 5V from USB. The output…
Part Number: TPS63000-Q1 Hi Team,
1) Does TPS63000-Q1 have Dynamic Voltage Positioning function? 2) If yes, what is the variation range(max, typ, min)?
Although it is not listed the data sheet, I posted this question because TP63060 of the same series…
Part Number: TPS63000 Other Parts Discussed in Thread: TPS63900 , TPS631000 The input voltage range of our products is 3.0V ~ 4.4V and the output is 3.6V. When the input voltage is 4V ~ 4.4V and 3V ~ 3.4V, the ripple is normal. When the input voltage is…
Part Number: TPS63000-Q1 Hi Team,
Does Cout(Output Capacitor) have Max value? Equation to calculate Min value is specified but to calculate Max value is not specified in the data sheet.
Best Regards,