Part Number: TPS63000 Other Parts Discussed in Thread: TPS63020 Hello team,
My customer is verifying the behavior when R1 removing or R2 shorting between GND and FB. In these case, Vout is calculated as max value from equation 1 in datasheet. This should…
Part Number: TPS63000 Hi all
I have an odd (and urgent!) issue with a design using the TPS63000; it is set up to give an output voltage of 3.6V, and although I've just noticed the ground fill on the top layer did not connect to the exposed pad on the…
Part Number: TPS63000 Hi Guys
Customer asked:
We have a battery powered device (using - 2 X 1.5V Alkaline Cells) that uses the TI 63000 step-up switcher (3.3V fixed output).
Under low load/standby condition this device draws 3mA.
The spec shows device…
Part Number: TPS63000-Q1 Other Parts Discussed in Thread: TPS63020-Q1 Hi Sir,
TPS63000IDRCRQ1 datasheet only show this description "Qualified for Automotive application",
We need to note the documents with AEC-Q100, Please help to provide, …
Part Number: TPS63000 Data sheet (Section 8.2.2.1, page 11) has Equation 2 for computing the value of feedforward capacitor. If R1 is 1Megohm, then Cff=2.2uF. This seems like a very large number. Can you please confirm that there is not a factor of 1…
Hi Miguel,
I am afraid we do not have a BUBO to fully meet your request.
For low Vin BUBO, i mean 5.5V lower, we have only TPS63000 and TPS63020 have AEC-Q100 compliant.
For middle Vin BUBO, we can not support 2.5Vin, if my remember is correct, minimum…
Part Number: BQ25300 Other Parts Discussed in Thread: TPS63000 Tool/software: Hellow.
When the battery is in UVP (under voltage protection) state, it does not charge.
(When it is not in UVP state, it works normally.)
However , when I disable the DCDC…
Hi Maur í cio
Looking for your feedback about the test.
Also, attach the publications about methods to generate adjustable output for your reference: Dynamically Adjustable Output Using TPS63000 ,
The Figure 5 in Methods of output-voltage adjustment for…