Part Number: TPS63000 Other Parts Discussed in Thread: TPS63070 , TPS63050 Hi,
20% of my boards do not properly start. I use a PS (3.67V) with serial resistance to simulate a battery.
80% of my boards starts even if the serial resistance is 20ohms (10ohm…
Part Number: TPS63000 Hi Everyone
I'm using a a TPS63000 to provide a 3.5V supply from a Lithium Ion cell.
The cell voltage may be between 3.0 and 4.2 volts so the device may be working in boost or buck.
I'm finding that the current increases to around…
Part Number: TPS63000 I am using a TPS63000 in the following circuit - attempting to make a buck/boost converter to take a single cell lipo in and set for 3.0v on the output.
However, the output voltage is widely variable depending on the input voltage…
Part Number: TPS63000 We are using the TPS63000 to regulate the circuit supply voltage around 3.45V as shown in the image below:
PCB layout:
The supply voltage comes from a 3.7V LIPO battery or a 5.0V USB port.
The circuit was designed following the…
Hi, Could you please explain what do you mean by recommended tests for pin compatibility? The TPS63805 (chip-scale package) or the TPS63802 (DFN package) can be used in the same way as the TPS63000. Just make sure that the device operates in forced PWM…
Part Number: TPS63000 Dear,
our client RFQ TPS63000, if our desgin is input USB 5V, it`s could be workable?
condition A: battery input Voltage Range is 2.7V to 4.2V , Vo/Io= 3.3V/1A
condition B: input 5V USB
if any suggestion, Please advise me.
Thanks…
Part Number: TPS63000 Other Parts Discussed in Thread: TPS63802 Hi, Could you tell me about TPS63000 UVLO spec? Input voltage drops momentarily in customer application. With that background, please tell me the time when UVLO is triggered. Regards, Yusuke …
Part Number: TPS63000 Other Parts Discussed in Thread: TPS63020
Equipment 3.6V battery power supply, found that the battery quickly lost power, board MCU, TPS63000, wireless module several chips, test wireless module working current 100mA, not working…
Part Number: TPS63000
Dear TI-Team,
actually, I'm not that much a hardware guy. I'm just building hardware to get our software running on it. So I was happy to see that there is a WeBench TPS63000 customizer / power designer.
Our requirement is…
Part Number: TPS63000 Dear support member,
My customer used TPS63000.
I have two question.
Q1 Is there EMI data for TPS63000EVM?
Q2 Is there an application note about EMI countermeasures?
Best regard. Bob Lee.