Part Number: TPS63000-Q1 Other Parts Discussed in Thread: TPS63020-Q1 Hi Sir,
TPS63000IDRCRQ1 datasheet only show this description "Qualified for Automotive application",
We need to note the documents with AEC-Q100, Please help to provide, thanks…
Part Number: TPS63000-Q1 Other Parts Discussed in Thread: TPS63000 Dear Team,
May I know what's the with Rj-c , Rj-b , Ψj-t parameter of TPS63000-Q1?
It should be different from TPS63000 because the Rj-a are different.
Thanks
Shaq
Part Number: TPS63000 I am using a TPS63000 in the following circuit - attempting to make a buck/boost converter to take a single cell lipo in and set for 3.0v on the output.
However, the output voltage is widely variable depending on the input…
Other Parts Discussed in Thread: TPS63000 , TPS63000-Q1 Hello,
We use the TPS63000DRCT in our design (low power device) as a power supply.
Now for us, the quiescent current is very important (we use the low power save mode, pin #7 pulled low)
Our…
Please look at the TPIC74100-Q1, which is a Buck-Boost that generates 2 fixed 5V output rails (VOUT and 5Vg). It is a buck-boost (step-up and step-down converter) with a VIN range from 1.5-40V
If you need to generate a voltage other than 5V, I suggest…
Part Number: TPS63020-Q1 Other Parts Discussed in Thread: BQ25798 , , TPS63020 , TPS63000 Tool/software: Hello!
We need to obtain 3.3V from a 1S1P Li-Ion battery pack, using a BQ25798 as charger.
The problem is that when the battery is not connected…
Part Number: TPS63000 Hello guys,
One of my customers is considering using TPS63000 for their new products.
They have the following questions.
Could you please give me your reply for them?
Q1. There is a situation in the new products that the…
Part Number: TPS63000 Hello.
I use TPS63000 and have some questions.
Condition1. Current conspumtion is under 100mA.
Condition2. Input voltage is 5.0v and Output voltage is 3.3V .
Q1. There is high frequency sound, when I touch by hand on…
Part Number: TPS63000 Hi support team.
I have 2 questions.
Q1: I want to shut down a circuit when the battery voltage (VIN) is lower than the target value which higer than the under voltage lockout threshold.
In this case, is it correct way…
Part Number: TPS63000 Dear support member,
My customer used TPS63000.
I have two question.
Q1 Is there EMI data for TPS63000EVM?
Q2 Is there an application note about EMI countermeasures?
Best regard. Bob Lee.