Part Number: TPS63001 Tool/software: Dear Specialists,
My customer is evaluating TPS63001 and has a question.
I would be grateful if you could advise.
---
Does the current limit function in Power-Save Mode?
It has been observed that switching…
Part Number: TPS63001 Tool/software: Hi,
Output of TPS63001DRCR is going to connect with Vin of LP3874EMP-ADJ/NOPB and TLV70230QDSERQ1.
Do i need to use PTC fuse or other current protection? if i directly connect Vout with Vin of LP3874EMP-ADJ/NOPB…
Part Number: TPS63001 Tool/software: I am using the TPS63001 to supply my system. The input voltage to the module comes from a battery charger IC that, under operating conditions provides the battery voltage to the buck-boost. The TPS63001 becomes very…
Part Number: TPS63001
In the typical application, there is the addition of R3 & C4. What exactly is their purpose? Originally I thought it was just power filtering bypass capacitor (as recommended in the TPS6303) with a pullup resistor, but 100 ohms…
Part Number: TPS63001 what is the output of regulator TPS63001
this ic is giving 21. mA some thing output current is showing. i want to reduce this consumption in uA. how much current can be reduced in regulator ic from the circuit given below?
Part Number: TPS63001
Hi Ti Team,
From above application circuit if we increase the R3 value to 4.7K, does if effect the functionality of TPS63001?
If we use Resistor value 4.7K or higher, is there any issue with VINA (Supply voltage for control…
Part Number: TPS63001 Hi Ti Team,
We are facing the ripple issue in the output of the TPS63001 DRCR(3.3V fixed output). Please check the ripple captured image. The ripple variation is from 110 to 120mV with 100mA of load current.
Thanks & Regards…
Part Number: TPS63001
Short description: repeated failure of TPS63001
Email: seraged@ieee.org
Company: CAIRO UNIVERSITY
We are using TPS63001DRCR regulator to power a STM 32 micro controller board off a Li-ion battery.
The system is…
Part Number: TPS63001 Hello, I have used TPS63001DRTR in my design. Input Voltage- 4.2V ( Li-Ion Battery) Output voltage- 3.3V I am facing heating issue of TPS63001 even if at no load condition. At no load it is consuming 295mA current. I am not able…