Hello Jasper,
inductor partnumber is: CIGW252010GL2R2MNE from Samsung
By giving some moderate force finger taps I mean literally tapping with my finger on the other side of the board from the TPS63002 with moderate force. All components are on top…
Part Number: TPS63002 I am about to give up on this Product I've replaced the part several times watched my soldering heat and still cant get it to turn off using en pin. I take the pin to GND level and the output goes to 3.5v and wont turn off. Any Idea…
Part Number: TPS63002 Other Parts Discussed in Thread: TPS63802 Dear all,
I would like to ask about Power-On Current Consumption at VINA Pin.
In the data sheet, there is the following quiescent current (Iq), but there is no description of the current…
Part Number: TPS63002 Hello team,
My customer is evaluating TPS63002 circuitry using Webench schematic below(4.85Vin, 5Vout 1 Aout). However the circuitry didn't work well.
Could you please advise me why the TPS63002 circuitry doesn't work?
Evaluation…
Part Number: TPS63002 Other Parts Discussed in Thread: TPS63802 , TPS3803 Dear all,
I would like to ask a quesiton about this device
Our customer is planning to start with an input voltage of 3.6V with the following circuit diagram (R3 = R4 = 2kΩ…
Part Number: TPS63002 Other Parts Discussed in Thread: TPS63802
What do you recommend for a buck-boost regulator with I2C capabilities for adjusting the voltage outputs.
VIN range of 1.8 – 5.5V
Variable Vout range 3.3 – 5.5V
Iout: <2A
Maybe…
Part Number: TPS63002 I am using TPS63002 in one of the my project. I want to generate 5V @ 1A from Li-ion battry. So input is between 3 to 4.2 V. I have connected as shown below:
My issue is when i powered up IC getting hot output drops to…
Part Number: TPS63002 Hello! I'm designing a circuit using TPS63002. In recommended part list and application there is R100 resistor. I wonder if I can use R150 instead of R100 because I'd like to reduce BOM (I already have some R150 resistors in BOM…