Part Number: TPS63020 In TPS63020 datasheet the sample schematic show that the EN pin #12 is connected to GND through the capacitor C3.
Then in the WEBENCH Power Designer also displays the same schematic as in the datasheet. (i.e) EN pin #12 is connected…
Hi Raghavendra, Under those conditions you can expect around 5 mVpp ripple in PWM mode, and at most 90 mVpp outout voltage ripple in PFM (power save) mode. This is valid for our TPS63020EVM-487, and the output capacitors we have there. If you are using…
I just received a TPS63020EVM-487 and tried it.
The output is not steady, fluctuates about 50mV with the power save mode.
The output is stable when it is not in the power save mode.
The voltage is around 3.44V when in the power save mode and 3.29V when…
Part Number: TPS63020 Other Parts Discussed in Thread: PMP9759 , We are building a Peltier driver based on http://www.ti.com/tool/PMP9759 .
Our test circuit is not stable. We notice that the stability improves if low-impedance Peltiers are used (thus higher…
Hi Milos,
Thanks for the reply. I don't expect significant load transients, and efficiency isn't too important for me either. 25 mVpp is the DC ripple specification.
Unfortunately I am limited to a single 1206 on CIN and COUT due to PCBs already…
Part Number: TPS63020-Q1 Other Parts Discussed in Thread: TPS63020EVM-487 Hi
Our customer are going to estimate the start up time.
However there are no specification of the delay(startup) time on the datasheet.
How can we estimate the following delay or…
Other Parts Discussed in Thread: TPS63020EVM-487 , TPS63000 Hi
Our customer evaluates the TPS63020EVM. They found a overshoot at startup like the following waveform.
The problem is that the overshoot was larger than below. (The setting voltage is 3.3V.…
Other Parts Discussed in Thread: TPS63020 , TPS63020EVM-487 Hi
I have a question about over current limit operation of TPS63020.
I measured current limit operation with TI-EVVM (TPS63020EVM-487). However it was not such as what I expected.
I have confirmed…
Hi Florian-san
There are the condition. We don't get the waveform.
TPS63020EVM-487
fsw = 2.2MHz @External Sync clock
Vin = 3.5V, Vout=3.3V
Iout = 0.5A
Regards,
Koji Hamamoto
Other Parts Discussed in Thread: TPS63020 , TPS63020EVM-487 , TAS5615 Hi,
I'm working with TPS63020EVM-487. I have modified this PCB to my application, changing FB resistors to have 3,6V output voltage and inductor to make higher current output (1,5uH…