Part Number: TPS63030 Hi,
Could you please suggest any converters for TPS63030 which can be used as a replacement and also compatible with footprint, functionality and pinouts?
Regards,
Vino
Part Number: TPS63030
Is it possible to mention the maximum soft start delay from VEN high to VOUT valid?
For example, it does not exceed 1 msec.
<Conditions>
VIN: 3.0-5.5V
Operating temperature: -45-85 degree C
VOUT residual voltage: 0…
Part Number: TPS63030 Hi,
What is the expected behavior of this device if the EN pin is left floating? I don't see a clear indication in the datasheet of if there is a pullup/down on this pin internally.
Thanks,
Jose
Part Number: TPS63030 Other Parts Discussed in Thread: TPS63031 Hi,
Could you please suggest any converters for TPS63030 which can be used as a replacement and also compatible with footprint, functionality and pinouts?
Regards,
Vino
Part Number: TPS63030 Hi
I have a question about current limit protection of TPS63030.
If average switching current exceeded current limit, does this device shut down immediately or limit the current until operating thermal shut down?
Best…
Part Number: TPS63030 Other Parts Discussed in Thread: TPS62740 Hello, i have the following circuit
which is pretty much a copy of the one in the datasheet, with a small difference, the enable line is externally driven, in this case an atmega328p…
Part Number: TPS63030 Other Parts Discussed in Thread: TPS63802 Hello,
I'd like to ask whether TI has a buck-boost regulator similar with TPS63030 but with lower quiescent current value? Picture below is cut from TPS63030 DS.
Considering a…
Part Number: TPS63030 Other Parts Discussed in Thread: TPS63050 , Hi team,
I have a SMPS with output 5V(±100mV ripple, 4.9~5.1V) @ 600mA.
Now I choose TPS63030 (buck-boost) as the latter DC/DC to get 5V output with lower ripple (±50mV) @600mA.
It…
Hi Francesco, During the last part of the Li-ion charging (the constant voltage part) the charging is usually stopped once the battery current drops down to few percent of the initial charge current. 50 µA is much lower than this, so leaving the TPS63030…