Hi Adam,
TINA-TI model is available for TPS63020 and you can get it from below link.
TPS63020 TINA-TI Transient Reference Design
We do try to provide models at time of installation of TINA-TI and you can get some of them under Spice Macros Tab.…
Part Number: TPS63030 Other Parts Discussed in Thread: TPS63050 Hello,
I'm currently looking for a dcdc converter chip for our new product.
Our device runs on a battery which has a voltage from 2.5 to 4.2V. Directly connected to the battery is a motor…
Part Number: TPS63030 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models From the following link:
http://www.ti.com/product/TPS63030/toolssoftware
How do I utilize these PSPICE files in a TINA-TI simulation? Why are…
Hi,
I received the following question from my customer.
Does reverse current flow on the following condition?
VIn : 0V, EN : 0V, Vout : 3.3V
Best Regards,
Kuramochi
I've just had the same experience with my implementation of the TPS63030 boosting 3.3-4.5 volts to 4.0v. I was getting 177mVpp on the output! I tried 94uF caps on the output and 47uF on the input side. that make the waveform look like a triangle wave…
Part Number: TPS63030 I’m working on a project and I’ve incorporated the TPS63030 to regulate voltage coming off of a CR2032 battery. However, right now I’m just running off of a bench supply as I work out some of the issues in the system. The bench power…
I made a new board, this time with the PS/SYNC pin grounded. At first it was drawing 1mA but no output voltage was being generated. If I put a fairly large output cap on the board it would ramp up to the set output voltage then drop back to zero. I checked…
Other Parts Discussed in Thread: TPS63030 , TINA-TI , BQ25504 Hi,
for an exact test of my system I have to use the TPS63030. Where could I download Pspice, is there an open source also available?
Greetings,
Chris
This does sound odd. Without a Vin (if it really 0V), the Vout must be coming from somewhere else on the PCB. Common leakage paths include through pull-up resistors, MCU I/O pins, etc. Anything connected to Vin.
Just start measuring the voltage at…
Other Parts Discussed in Thread: TPS63030 , TPS63030EVM-417 Hello,
I have question about TPS63030 PS/SYNC Pin
There are 2 kinds of TPS63030 schematic as attached. One is TPS63030EVM-417 schematic and the other is schematic on TPS63030 datasheet…