Part Number: TPS63036 Hi Team,
A customer used TPS63036 as LED driver based on Figure 2 in the application notes below.
www.ti.com/.../slva419c.pdf
The device works normally at an input voltage of 2V. However at 5V input the LED has difficulty turning…
Part Number: TPS63036 Other Parts Discussed in Thread: TPS63060 Dear team,
Our TPS63036 has input voltage limit.
Do we have solution, which input range is 2~6V, output 4V/1A and Iq below 25uA?
Many Thanks
Jimmy
Part Number: TPS63036 Hi team, I'd like to know how to calculate the inductance value in the light load. My customer usually uses 70mA load. Condition Vin : TBD (4V~1.5V) Vout : 3.3V Iout(MAX) : 70mA At this time, how about capacitance value? Sincerely…
Part Number: TPS63036 Hi,
I've recently encountered a case of device triggered to shutdown on my circuitry & I've narrow down the potential root cause to TPS63036. Reason being that test of PCB was done under 55C temperature soak test with expected…
Part Number: TPS63036 HI TI Team:
I can see in the specification, that the output with PS/SYNC = GND can be +6% or -3% if IOUT < 5 mA .
If I understand ok, the accuraccy of the output would be better if IOUT > 5 mA but not worst, isn´t it? This behavior…
Part Number: TPS63036 Dears
My customer would like to use the external Frequency synchronization, but the range for external SYNC is 2.2 - 2.6MHz, the internal switching rage is 1.8- 2.2.
Customer want to know if they can use 2 MHz for external Frequency…
Part Number: TPS63036 I'm trying to get the most of the instantaneous power available from a lithium primary cell and, as it stands now, the efficiency is proving to be a bit of a roadblock. Like the person who made this post: e2e.ti.com/.../824651 ,…
Part Number: TPS63036 Other Parts Discussed in Thread: TPS63060 Hello,
I want to use TPS63036 Buck Boost Convertor for converting 3-6 V Input range to 5 V output. I am using two 3 V coin cells in series as Vtg source.
Is it OK if 6 V input is given…
Part Number: TPS63036 Hello Team,
Need your help to verify the stability analysis(BODE Analysis) report of TPS63036. Attached is the report for verification, please help with your comments. Can you please share the stability analysis report done with…