Part Number: TPS63036 Hi team,
where there is no WEBENCH for the part, can you help simulation below?Effiency and thermal simulation?
Vin:4.2-2.7V
Vout :3.3V
Iout: 150mA
Part Number: TPS63036 The tolerance of the voltage on pin FB given in the data sheet for room temperature only (page 3 of data sheet). I need to know the tolerance (or a temp coeff) across the entire operating temperature (-40 to 85C) in order to do error…
Part Number: TPS63036 HI TI Team:
The actual test efficiency is lower than that described in the specification,The data are shown in the annex document.
Please help to confirm whether the actual test data is normal ?Where will affected efficiency…
Part Number: TPS63036 Other Parts Discussed in Thread: TPS63031 hi all,
a customer of mine is looking at TPS63036.
he read there is a fixed Vout version (3.3V most likely), but I couldn't find it anywhere...
is a typo in datasheet?
i found the…
Hi Daniel,
Please find the attachment for the step model of TPS63036. The same will be available on ti.com in few days.
YFG0008APAL.zip
Thanks & Regards,
Praveen B
Hello again Sabrina.
Schematic and layout are same as in our "TPS63036 Start Up" forum exchange, starting 2016/04/25. Copied below for benefit of other forum readers: (Aside: That other exchange resolved with 50 mSec minimum shut down duration.) Back…
Sabrina- Thanks for your reply. An additional occurrence of the TPS63036 fail to restart yielded V3R3 at 0.049 Volts and TPS63036 pin C1 at 0.116 Volts average. Schematic: Layout: Four scope traces, with discussion following: 1) Enable and V3R3 with light…
Note: HTML that was referenced does not work - but it's not very critical. It was simply the part compare page for the 3 parts (024, 036, and 050).
Here's a screenshot instead.
imgh.us/compare_parts_buckboost.png
Other Parts Discussed in Thread: TPS63036 Hi,
where can we find the footprint for the TPS63036? It is a 8-pin WCSP - YFG (R-XBGA-N8) - 1.854 mm x 1.076 mm
Thanks
Rick