Part Number: TPS63051 Hi, Let's talk about the soft start and output voltage of the TPS63051. Customers are testing SS caps in the 10nF and 22nF patterns. In that test, the output voltage waveform started up while oscillating. Let me ask you two questions…
Part Number: TPS63051 Hi, Does TPS63051 have a pre-bias start up function? When the TPS63051 is externally turned ON/OFF, output discharge is slow and the voltage remains on the output side when restarting. If not, customer adds RC to the EN pin to specify…
Part Number: TPS63051 Dear E2E,
We would like to know the output accuracy in 3V3 input by using tps63051.
i didn't see the accuracy data in tps63051 datasheet at 3.3Vin.
Please help to provide the data.
Sincerely,
Jason
Part Number: TPS63051 Hi, Could you tell me about the slew rate requirement of the voltage applied to the EN pin? Since the rise of the input voltage is slow, it takes about 10 msec at maximum. Is there a problem if the slew rate is slow? If there is a problem…
Part Number: TPS63051 Dear E2E,
within our team we are using the TPS63051 in a Li-ion battery powered application within a custom miniaturized PCB, which needs 3V3 constant output voltage for powering all the components. I followed all the design suggestions…
Part Number: TPS63050 Other Parts Discussed in Thread: TPS63051 , Hi,
I didn't find the TPS63050 TINA- model, but I found the TPS63051 model.
So I use this model to simulate first. But when I try to see the DC-level first, I get the wrong Vout voltage…
Part Number: TPS63051 When I supply 3.7V to my buck-boost circuit the chip or the inductor starts ringing and the top of the chip starts to get very hot. The output of the circuit when i read it with a DMM is 0V. This is all done with no loading on the…
Part Number: TPS63051 Tool/software: WEBENCH® Design Tools Hi
I have exported a WebBench simulation model with steady-state solver and opened in a TINA.
If I run it with DC Analysis to check node voltage , I could not get it to desired out put.(3.3V) …
Part Number: TPS63051 Let me ask a quick question about TPS63051. Do we need care for leave open or connect to GND if we don't use the PG.
Thanks in advance. S.Sawamoto
Part Number: TPS63051 There are dimensions missing from package outline drawing "mxb343" for the YFF0012 DSBGA 12-ball package (4222191/A 07/2015). "D" and "E" (max dimensions of the part itself) have no data. Help?