Part Number: TPS63060 Tool/software: HI,
Title: Issue with TPS63060 Buck-Boost Converter – Output Voltage Fluctuation
Description: I am using the TPS63060 buck-boost converter with the following configuration:
EN (Enable) pin is directly connected…
Part Number: TPS63060 Tool/software: Hi,
I am using the TPS63060 buck-boost converter with the following configuration:
EN (Enable) pin is directly connected to VIN
PG (Power Good) pin is connected to GND
PS/SYNC pin is connected to VIN
Feedback resistor…
Part Number: TPS63060 Tool/software: Hi,Toe,
The TPS63060 PS/SYNC pin does not work when directly connected to ground, as I don't get any output voltage. However, when I connect it to the input voltage, it works, and I get the output voltage.
According…
Part Number: TPS63060 Tool/software: Hi support team,
The undershoot of L1 has a peak of about -2.0V over a period of 16ns.
Although it exceeds 10ns, can we assume that it is not a problem because the effective value is low?
Regards,
Dice-K
Part Number: TPS63060 Tool/software: Hi team,
Let me double check behavior of PG pin.
It only becomes low when average inductor current exceeds internal current limit value and it doesn't change state for over voltage condition.
Is this understanding…
Part Number: TPS63060 Tool/software:
The starting current of the tps63060 is 2.4A, the input voltage is 6V, and the output is 5V. Is it normal?
The problem now is that the input power supply is an alkaline battery. When TPS63060 starts, the current…
Part Number: TPS63060 Tool/software: Hi support team,
When starting the TPS63060 with the settings VIN: 7.2V VOUT: 5.2V, the SW stops for a while after starting, and then starts again.
ch1: Input voltage 7.2V (out of range, not shown) ch2: DCDC output…
Part Number: TPS63060 Tool/software: Hello,
On the datasheet for the TPS6306x parts, I can't seem to find a specification for the voltage threshold levels on the device enable (EN) pin. It just references "high" / "low" or "1" / "0". This is being…
Part Number: TPS63060 Tool/software: Hello, I am an FAE at a distributor that handles TI products. I received the following question from a customer.
I would like to ask about the "PG output low voltage" listed on the datasheet. Under TEST CONDITIONS…