Part Number: TPS63060-EP Other Parts Discussed in Thread: TPS63060 Tool/software: Can the TPS63060MDSCTEP be made to perform to a tighter frequency range (is 1.850 MHz to 3.0 MHz). We have interference issues at certain frequencies.
Part Number: TPS63060-EP Other Parts Discussed in Thread: TPS63060 , Hi Team,
Our customer is looking for the electrical characteristics of TPS63060MDSCTEP as follows:
1.Maximum reverse current 2.Time from PS/SYNC pin going low to start operating…
Part Number: TPS63060-EP Other Parts Discussed in Thread: TPS63060 Hello,
Would it be legal to add a charge pump to TPS63060 to create a +/-7.5V supplies? I know it doesn't use an external rectifier which would make it easier. If yes, should I add it…
Part Number: TPS63060-EP Hello,
Please suggest an automotive equivalent for TPS63060-EP.
The requirements are Vin 1.8-3.7V, 1A current, AECQ qualified,-55 to125C,Vout is 3.3V
Part Number: LM25118-Q1 Other Parts Discussed in Thread: LM25118 , TPS63060-EP Hi Team,
Could you help? I'm posting this in behalf of the customer.
I'm interested in the LM25118 pwm chip that TI offer's, specifically because it is catered to a buck…
Hi 5818977,
Are you referring to max. ambient temperature of 125C? The maximum recommended junction temperature for the TPS63060-EP is 125C. As for the vibration and pressure specifications, I will check it, but I doubt there are such specifications…
Absolutely NOT... Max Vin is 5.5 V !!
This part seems to be a solution
www.ti.com/.../tps63060-ep
but has a Vin(max) of 12V, so you could be forced to limit the input voltage, by some means.
Otherwise, a bit more complex, but...
Something like…