Part Number: TPS63061 Other Parts Discussed in Thread: TPS63060 When the input voltage was applied to the Vin terminal as shown below, the Vout voltage was not output by method (1).
(1) Apply 6V voltage of 4 alkaline AA batteries to Vin by switching…
Hi Milos,
Many thanks for the quick response. I was able to take a few measurements again . I will show you .
1、The diagram bellow shows power rail in my design.
2、This picture was shown DC power supply .
3、This picture was shown waveform of L1…
Part Number: TPS63061 HI
Would like to check if this waveform observed by my customer is correct?
Vin = 5V
Is the Vout max is abit high?
Vout is shown below
INg
Part Number: TPS63061 Hi,
we are using TPS63061 to convert input voltages from 1S or 2S li-ions (=2.7-8.4V) to output 5V USB. When the input or output is disconnected and connected several times, chip fails and eventually shorts. It happen same when…
Part Number: TPS63061 Hello,
The TPS63061 clearly specifies "Due to the 4-switch topology, the load is always disconnected from the input during shutdown of the
converter".
On our design the issue is that the input power supply could goes down because…
Hi Jack, We haven’t heard back so we're assuming this resolves your issue. If not, just post a reply below, or create a new thread if the thread has locked due to time-out. Thanks and regards, Milos
Part Number: TPS63061 Other Parts Discussed in Thread: LM5175 , TPS63070 , LM5118 , LM25118 Hi Team,
Please help me with TI Part which meets below specs:
Price/Unit: <2$, for MOQ 1000
Input voltage range: 5V to 12.6V (battery source)
Output…
Part Number: TPS63061 Since there is a worldwide critical shortage of large-value ceramic caps. We currently use a pair of 47µF 25V ceramic output caps in our TPS63061 implementation, plus a third one at a remote location, which is switched by a MOSFET…
Part Number: TPS63061 Hi! We are using this chip for battery powered application. Device has two options, either 4x AA or 8xAA battery on the input. We have realtively small batch of these devices made, all were functionally tested in house, then shipped…