Part Number: TPS63070 (this is my previous question in E2E ; https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1086052/tps63070-cannot-simulate-on-webench )
Hello TI experts,
my customer considers TPS63070…
Part Number: TPS63070 Dear Support,
in the data sheet of the recommended inductor part XFL4020-152MEC from Coilcraft I found the information that pin 1 of the inductor is the start (short) lead and that high dv/dt should be connected here for lowest…
Part Number: TPS63070 Dears,
TPS630701 is used in the customer's project, and when this material is powered on again, the instantaneous current reaches 1.2A, if this value can be reduced through some modifications,tks!
Part Number: TPS63070 Hi Team,
As I am performing load transient analysis for TPS63070 using the circuit attached, I observed a unwanted voltage dip in input voltage. I want to avoid or minimize the voltage dip in input voltage. To achieve this please…
Part Number: TPS63070 Other Parts Discussed in Thread: PMP9796 , TPS55288 Dear team,
I would like to use TPS63070 as a TEC driver. but there are some issue.
As PMP9796, The TEC voltage can be varied between -2.5 ~ 4V . but the customer want to design…
Part Number: TPS63070 Other Parts Discussed in Thread: TPS63060 Hello TI experts,
my customer wants to use TPS63070 for their new product.
the conditions of customer are as below;
input : 2.7V ~ 12V
output : 5V/1A or 6V/1A
I confirmed that 5V…