Part Number: TPS631010 I designed a 3V to 1.8V dc-dc regulator and 3V to 3.3V dc-dc regulator using TPS631010YBGR (buck-boost regulator).
A maximum current of 51.1mA is drawn from 1.8V regulator and 240mA from 3.3V regulator. The 3.3V regulator supplies…
Part Number: TPS631010 Hi,
Currently we are developing a product which uses the above voltage regulator, output voltage being 1.8V. It powers an MCU with a current consumption of 10mA during active mode and 200uA during sleep mode. How does this affect…
Part Number: TPS631010
Hello,
I would like to ask you about the input overvoltage protection of the TPS631010. What is the behavior of the device when overvoltage (VT+(IVP)) is applied to the input side? What is the state of VOUT when overvoltage is applied…
Part Number: TPS631010 Hi Team,
Do we have thermal snapshots of TPS631010? I believed I saw some user manuals for EVBM with this information. The test condition is below. Thank you.
Load current is 2.0A. Vin is 3.4V. Vout is 3.65V.
Best regards,
Mike
Part Number: TPS631010 Other Parts Discussed in Thread: TPS61033 Hi,
Looking for the minimum and maximum DutyCycle of the TPS631010 in Forced PWM (FPWM) Mode. Or minimum On-Time of the switches. Couldn't find it in the Datasheet December 2022, did i missed…
Part Number: TPS63030 Other Parts Discussed in Thread: TPS631010 , TPS631000 Tool/software: We need an alternative buck-boost converter IC with the same pinout and footprint but better output current, upto 1.5A supporting IC. Please suggest us options…
Hi Shunsuke,
TPSM83100 is just the module version of TPS631010. And we have Webench for TPS631010 available in link below.
https://webench.ti.com/power-designer/switching-regulator/customize/20?noparams=0
Regards
Tao