Part Number: TPS63710 Tool/software: Dear Specialists,
My customer is considering TPS63710 and has a question.
I would be grateful if you could advise.
---
I am considering using the TPS63710 to generate -5V (10mA) from +9V.
I believe that since…
Part Number: TPS63710 Hi,
Below is my schematic arround TPS7A3301RGWT for my custom board, i have tried to maximum follow the EVK
But still i wish to know if there are any flaws in my layout
Kindly have a look and drop your valuabel comments
Schematic…
Part Number: TPS63710 Other Parts Discussed in Thread: TPS62903 Tool/software: Hi team,
my customer wants a product to do Vin:5~12V , Vout: -5V , Iout=0.4A and the precision needs to be less than 1%.
Customer has chosen TPS63710 but the maximum duty…
Part Number: TPS63710 Other Parts Discussed in Thread: LMR51610-Q1 Tool/software: I need a converter which converts +24V to -15V.Kindly provide me with a list of parts that matches the above specification.
Part Number: TPS63710 Other Parts Discussed in Thread: TPS629203 Tool/software: Hi team,
What is the best option for below request?
Vin=3.3V
Vout=-2.0V
Imax=105mA
With EN function
small size
high efficiency
Low Iq
Thanks!
Jayden…
Part Number: TPS63710 Other Parts Discussed in Thread: TPS62903 , TPS62135 Hi Team,
I would like to double check with you that the quiescent current of TPS63710, is it 15mA but not 15uA? Thanks
Sincerely
Frank
Part Number: TPS63710 Hello,
I am planning to use TPS63710 to obtain -3.3V from a 5V input. According to the datasheet, as long as 5V > 0.7x|3.3V|,
there should be no issues. Please confirm this for me.
I am currently using the TPS63710 to generate…
Part Number: TPS63710 Tool/software: Hi !
I'm Matis,
An apprentice Engineer, currently working on the design of a power electronics board.
Context :
We're using a 6-layer PCB, with just over a dozen of the MOSFETs IAUT300N10S5N015ATMA1 from…
Part Number: TPS63710 Other Parts Discussed in Thread: TPS62912
Hi,
I have a power rail requirement of below
Polarity
Voltage
Load Current
+
2.5
400
mA
-
2.5
400
mA
+
5
620
mA
-
5
330 …
Part Number: TPS63710 Hello,
There is a parameter tdelay in the datasheet, which is defined as the delay between the moment EN-pin is asserted HIGH and the moment the switching starts. There is no formula for it. Just a number given in the table of…