Hi Alex,
it should be Ok in normal condition. as the FB is closed to the edge of the PCB and the FB pin has high input impedance. please make sure not touching this pin and care about the ESD event into the pin.
Part Number: TPS63806 Other Parts Discussed in Thread: TPS552882 Hi Team,
My customer is surveying our buck-boost solution now,
They need:
Input voltage : 1 cell battery (3V~4.4V)
Output voltage : fixed 3.3V
Output current : Imax = 3A
…
Hi Dawei, Considering the load transient requirements, the TPS63806 is the best fit. The shutdown current is 45 nA typically, 600 nA maximum. Best regards, Milos
Part Number: TPS63806 Currently I want to use TPS63806 to drive LED with 3.4A .Input is 3.6V,output requires 3.7V 3.4A.My control logic is that connect the IC FB pin with a RC(24K,1uF) circuitry, that MCU output a 8K PWM to one side of the R r adjusting…
Part Number: BQ25622E Other Parts Discussed in Thread: TPS63806 , Tool/software: Hi
Requirements: VBUS 5V input >Charger IC >PowerPath >SYS >Boost DC/DC > Vout 5V @3A Is it feasible for us to choose BQ25622E + TPS63806?
Part Number: TPS630250 Other Parts Discussed in Thread: TPS63806 Tool/software: Dear Technical Team,
I am looking for a buck-boost converter which can provide 3A or more to its output (only 1 output required).
I found several products of your catalogue…