Part Number: TPS63806 Hi,
In our application, TPS63086 is selected to meet requirements below, at the moment, is it the best PN?
1, Input: 3.3V - 3.8V (Li-Ion rechargeable battery).
2, Output: 3.8V (typical), maximum 400mv voltage drop for load 2A pulse…
Hi Abhineet,
For this power request, currently TPS552892 is most suitable, but the Vin rising voltage is 3.0V max, it means the device could only startup with higher than 3.0Vin, but can support 2.7Vin falling voltage.
Apart from TPS552892, you can also…
Part Number: TPS63806 Currently I want to use TPS63806 to drive LED with 3.4A .Input is 3.6V,output requires 3.7V 3.4A.My control logic is that connect the IC FB pin with a RC(24K,1uF) circuitry, that MCU output a 8K PWM to one side of the R r adjusting…
Hi Ignacio,
Ok, i would like to recommend our TPS63806 .
For LC filter, yes, you can have a LC filter to take care the 5Mhz noise, such as a 1uH+1uF LC filter after output cap. The inrush current should smaller than 4A with TPS63806.
Regards
Tao
Hi Kenny,
Because 3A is out of current capability for one BUBO converter. TPS63806 is our BUBO device with highest output current capability.
Regards
Tao
Hi Andres,
Can you take a look at TPS63806, it output capability is little stronger than TPS63802.
My concern about two device in parallel is the balance between this two device. As you know, there is a variation of reference voltage internal, resister…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: TPS63806
Tool/software:
Hi team,
I am trying to run a PSPICE for TI simulation based on the transient with the diode spice model downloaded from official website of ONSEMI.
The diode part number…
Part Number: TPS61023 Other Parts Discussed in Thread: BQ25302 , TPS63806 , TPS22995 Hi team,
This issue extends from previous issue .
Description
I have decided to add a new power supply IC(TPS61023) dedicated to supplying power to piezoelectric devices…
Part Number: TPS63802 Other Parts Discussed in Thread: TPS63000 , TPS63806 , Hi expert,
TPS63000 is usually used as TEC driver, but its output can not sink much current. I would like to see the sink current capability of TPS63802 and TPS63806.
Thanks.