Part Number: TPS63810 Hi Ti team,
No load test TPS63810 startup voltage, found that the lowest startup voltage is 2.5V, specification is 2.2V.( Not in the EVM),Please help to confirm,Thanks!
Part Number: TPS63810 Hi Team,
my customer want to use GPIO to control Vsel and found there are below parameters? does it mean the output current capablity of GPIO should be above the value to drive VIH or VIL ? Thanks.
For example, if GPIO has 10uA…
Part Number: TPS63810 Dear Team, we are having an issue with the output power of TPS63810 when attached to an Iridium SBD9603N modem (Please see specifications attached on page 21). This modem needs 5.0 V and up to 1.3A peak power, and randomly the output…
Part Number: TPS63810 HI team,
sometimes, at sharp load changes chip falls to abnormal state, unable to maintain stable output voltage, output generates spikes. And chip will retain this state permanently, initialization/refreshing voltage settings…
Part Number: TPS63810 Dear TI,
In the datasheet, TI strongly recommend an 0.47uH inductor to be chosen for TPS63810. Here we want to check with you if we can use an 1uH inductor? Is there any risk, such as loop stability? In our design, Vin is the…
Part Number: TPS63810 Hi Team,
Just want to check if there is bypass mode when Vin=Vout.
in datasheet, I see when Vin=Vout, it changes between buck, boost and Commutate phase. Only in commutate phase, it is similar with bypass mode. But it cannot…