Other Parts Discussed in Thread: TPS63811 Hello,
My customer would like to have SCL and SDA pins IBIS model to simulate TPS63811 I2C interface.
But, TPS63811 product line does not have the IBIS model for this device. (Please refer to the following…
Hello Yichen, Minqiu,
I have retried today in Webench power designer, now it work (I don't undertand why last week it did not work).
Thanks for the answers.
Best regards.
thierry
Part Number: TPS63810 Other Parts Discussed in Thread: TPS63811 , Hi Team,
Just want to check if TPS63810 and TPS63811 has same die and only difference is because of different trim in Fab. Thanks.
BRs
Given
Part Number: TPS63811 Other Parts Discussed in Thread: TPS55288 Hi All,
TPS63811 input is only 2.2V~5.5V.
Is there any device like TPS63811 which output voltage can set by I2C?
requirements are as fellow:
Vin=3V~9V
Vout can set by I2C
Iout…
Part Number: TPS63811 Hello,
Looks like efficiency graphs and load transient response graphs for PWM mode are missed in the datasheet. Any way to see it?
Thanks,
Eugene
Part Number: TPS63806 Other Parts Discussed in Thread: TPS63811 Tool/software: Hi team,
do we have product to support below request?
VIN
2V~5V
VOUT
need support 4.2V
IOUT
support 3A
Efficiency
90.00%@VIN=3V…
Part Number: TPS63811EVM Other Parts Discussed in Thread: TPS63810 , USB2ANY , TPS63810EVM , TPS63811 I am using an Arduino MEGA2560_R3 with TPS63811EVM module, communication via I2C (Wire library). I am able to write to device registers but seem to be…
Other Parts Discussed in Thread: TPS63811 Hi team,
My customer request for a buck-boost device which has below demand. They use it for OIS.
Vout range: 1.5 - 3.3V
Step: min 50mV, max 1.5V.
Vout regulation accuracy:10mV
Vout regulation slew rate…
Part Number: TPS2597 Other Parts Discussed in Thread: TPS63811 We are using the TPS25974L in the circuit shown below:
The output of the eFuse is connected to circuitry that includes 380uF of capacitance.
When the eFuse is enabled we see a current…