Part Number: TPS63900 Other Parts Discussed in Thread: LMP7721 TPS63900 TPS7A2030 LMP7721 MAX3223EIPWR TPS7A2030 Are the products with the model numbers listed above recommended for new designs?
If not, could you please suggest some alternatives?
…
Part Number: TPS63900 Hi team,
My customer would like to adjust the inrush with 3V7 at 70mA. There are resistor settings for 50mA and 100mA. I also read that the the device is only reading teh settings at start-up. A resistor setting for 70mA maybe…
Part Number: TPS63900 Hello,
I am working on a design using TPS63900 as a Boost and I would like your opinion about an issue we have detected
In our design power supply is a 2 cell ER18505H + SCP1520A pack 3.7V
the pack is connected to TPS63900…
Part Number: TPS63900 Hi TI team,
I am evaluating the TPS63900 buck-boost converter for a low-power embedded system and have observed an unexpected behavior when operating close to the minimum input voltage.
My requirement is to generate 3.3 V from…
Part Number: TPS63900 I am designing an NB-IoT / LTE-M design using the TPS63900 to power an nRF9151 from a battery, with a supercapacitor at the output of the DC/DC to support TX bursts. I would like to confirm whether my intended use of the TPS63900…
Part Number: TPS63900
HI TI,
I have used the TPS63900 chip and successfully constructed a power supply circuit. However, since our equipment will undergo single-fault testing during CE testing, during which the pins of this chip may be randomly…
Part Number: TPS63900 Tool/software: Hi Team,
I am using TPS63900 as an input voltage of 3.3 V and an output voltage of 3.3 V. The datasheet says that the accuracy of the output voltage is ±1.5%, so I thought that would be the case, but when I actually…
Part Number: TPS63900 Hi I already exposed my case on ticket TPS63900: TPS63900 failure - Power management forum - Power management - TI E2E support forums a month ago, but I can continue with the thread so I create this new ticket to give some new informations…
Part Number: TPS63900 FIRSTTRY.DSN
Tool/software:
Hello everyone,
I used Pspice for the first time. Before that I always used LTspice, but the model of the TPS63900 was only available in PSpice.
The goal is to generate an output voltage of 3…
Part Number: TPS63900 Tool/software: I am using TPS63900 Is Buck Mode. Input Voltage as 4.2V and Output Voltage at 3.3V. Load current as 0.5A. I want to calculate peak current through the I.C. and Inductor and for that I need to know the tw:A; , tw(B…