Part Number: TPS63901
Hi,
When simulating in PSpice, placing an Rcfg causes the error “less than 2 connections at node NO*** (Node in CFG1 to CFG3)”. How should this be addressed?
VO1=3.3V, VO2=1.8V, ICL=10mA
Regards,
Max
Part Number: TPS63901 Tool/software: The package size of this product we tested is not consistent with the datasheet. The datasheet is L:MAX1.49mm,MIN1.43mm W:MAX1.14mm,MIN1.08mm, but our measurement is L:1.513mm,1.525mm, W:1.156mm,1.162mm
Could you…
Part Number: TPS63901 Tool/software: Hi team,
This (TPS63901YCJR) IC is not giving an output of 3.3 V. It always gives 1.8 V. According to the schematic, if I set the SEL pin high, it should give 1.8 V, and if I set the SEL pin low, it should give 3…
Part Number: TPS63901 Tool/software: I am calculating the inductor peak current parameter so that I can select appropriate inductor for my application. But in Equation5 of the datasheet, We need duty cycle value in boost mode. But I could not find duty…
Part Number: TPS63901 Tool/software: Hi support team, Currently being evaluated with TPS63901EVM.
I checked the operation during soft-start and found something that concerned me.
TPS63901_Soft-Start_250509.xlsx It is set to increase from 1.8V to the…
Part Number: TPS63901 Other Parts Discussed in Thread: TPS631010 , , TPS63900 Tool/software: Hi support team,
I'd like to compare the TPS63901 and TPS631010 to see which has lower power consumption.
The TPS63901 does not have a definition for "Quiescent…
Part Number: TPS63901 Tool/software: Hi team,
Could we get this schematic reviewed?
My customer is seeing an issue that the device is delivering an output even with the enable low and had posted their question on E2E. I want to have their schematic…
Part Number: TPS63901
Tool/software:
Hi I've got a design with two instances of TPS63901 buck boost converter. One is 5 to 3.6V and the other is 5 to 5V. (The input 5V can go down to 2.5V so that's why the application uses buck boost). For both circuits…