Part Number: TPS65000
hi,
I have a question about over current protection.
How to achieve protection mechanism?
datasheet only write as below:
Fixed output voltages and additional current limit options are also possible. Contact TI for further information…
Hi Frank,
Thanks for the feedback. Since this is not an automotive application, how about this low-voltage 3 channel PMIC: TPS65000 data sheet, product information and support | TI.com
It is 1 DCDC + 2 LDO with output voltage set by external feedback resistors…
Part Number: TPS65000 HI:
Our products use the TPS65000RTER as the system power supply, from the product development stage to the final mass production stage, often encountered the chip damage situation(More than a hundred samples), the abnormal phenomenon…
Other Parts Discussed in Thread: TPS65000 Iwould like to confirm the thermal simulation model.
The customer wants the thermal simulation (thermal hydraulics, heat flow) with TPS65000.
Do you have the thermal simulation model (like DELPHI model) for TPS65000…
Hi Marvin,
Best option is to use the TPS65000 which does not include SVS.
For not using SVS in TPS65001, ground MR, RST, RSTSNS, and float TRST.
Thanks,
Daniel W
Hi,
For 12V applications the TPS650330-Q1 is recommended. Please refer to the product page and FAQs for information on this device.
https://www.ti.com/product/TPS650330-Q1
https://e2e.ti.com/search?q=tps650330&category=forum&faq=true
For 24V applications…
Other Parts Discussed in Thread: TPS65000 , TPS65000EVM-469 In TPS65000's Data sheet, the following description in Pin Function about PGND and AGND are very unclear.
[Power ground – Connected to the PowerPAD™]
[Analog ground - Star…
Part Number: TPS65720 Other Parts Discussed in Thread: TPS65217 , TPS65218D0 , TPS65000-Q1 Hello,
I don't see a PSRR spec for the integrated LDO, we want to use this on a noise sensitive rail. Where can I find this spec?
Thanks, Nick
Part Number: TPS65311-Q1 Other Parts Discussed in Thread: TPS62160-Q1 , TPS65000-Q1 Hi team,
For this specific requirement in camera ADAS system, 4 in 1 PMIC devices recommendation, TPS65311-Q1 is 8*8 package. Is there any other smaller size (like 3*3) recommentdation…
Hi Randy,
Not with built in clock generation. The TPS65000 could support power for an external clock as well as the imager rails.
Best Regards,
Rick S.