Part Number: TPS65000-Q1 Hi,
We have received a request from our customer to review the schematic related to this device.
However, due to confidentiality and security restrictions, we are not able to upload these materials
Thanks
Part Number: TPS65000-Q1
Tool/software:
Dear Team,
Can I get to know whether there are any similar IC TPS65000TRTERQ1 are available with 3 output as LDO. I need 2.8V , 1.8V and 1.15V with all as LDO, because of the compact size we cant add any inductor…
Part Number: TPS65000-Q1 Other Parts Discussed in Thread: TPS65000 Tool/software:
Why does the DC-DC converter integrated in the TPS65000 experience a brief output interruption when switching from PFM mode to PWM mode?
At this time, the shutdown…
Part Number: TPS65000-Q1 Hi team,
mu customer use this device, the output sequence of VOUT is: 2.9V first works, then 1.8V, and finally 1.1V, but according to actual circuit test, 1.1V normal output, However, the 2.9V and 1.8V outputs were abnormal…
Part Number: TPS65000-Q1 Hello Experts,
Can you help to understand what happens to TPS65000-Q1 DC/DC output when VINDCDC rises up (system starts) and falls down (system shuts down) in <0V - >=2.3V> range?
Datasheet gives:
UVLO at 1.72V ~ 1.82V…
Part Number: TPS65000-Q1 Other Parts Discussed in Thread: TPS650330-Q1 Hi team,
My customer requires PMIC for below power supply requirement.
- Vin = 5V+/- 0.2V
- 1.2V : 310mA max
- 1.8V: 227mA max
- 2.8V: 40mA max
- Ta= 95degC
Is there…
Part Number: TPS65000-Q1 Other Parts Discussed in Thread: TPS650330-Q1 Hello, may I know TPS65000-Q1's next generation PMIC P/N (ASIL-B compliant)? I saw the introduction from web seminar, but I can't find the data from ti.com. Thanks!
Part Number: TPS65000-Q1 Hi Team!
I have few questions about TPS65000-Q1 regulation accuracy:
Are datasheet DCDC accuracy numbers (+/-1.5%) given for whole operating ambient temperature range (-40 / +105 degC)?
To calculate DCDC accuracy, the…
Part Number: TPS65000-Q1 Other Parts Discussed in Thread: TPS650330-Q1 , TIDA-020002 , TIDA-020003 Hi Team,
I'd like to use this part to replace discrete power solution, but I'd like to know, how this LDO avoid the ripple noise from buck?
In the original…
Part Number: TPS65000-Q1 Other Parts Discussed in Thread: TINA-TI Hi Team, My customer considers to use TPS65000-Q1. He wants to confirm ramp-up time of VDCDC and VLDOx in simulation although the datasheet shows typical value. Is there simulation mode…