The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: TPS65023 Hi team,
My customer is searching for a power supply solution for Xilinx XCZU4CG. I checked Webench and it recommends TPS65023. But I just want to double check if TPS65023 is suitable for XCZU4CG? And do we have any reference design…
Hello Emily,
Sorry for waiting as I've just received feedback from client as follows:
For your information.
Thank you for your support.
Regards, Archie A.
Hello,
Thank you for the explanation. I have a few follow up questions.
Are all of the connections in the diagram you posted required to use IPG-UI and the MSP430F5529 Launchpad when programming in circuit:
P4.1 I2C_SDA <--> SDA
P4.2 I2…
Part Number: TPS65023 Other Parts Discussed in Thread: TMS320C6748 , TMS320C6742 , OMAP-L138 Hello guys,
One of my customers is considering using TPS65023 as a power supply for TMS320C6748.
They found the follwowing application note which was written to…
Part Number: TPS65023 Other Parts Discussed in Thread: TPS650250
Hi,
we use all 3 DCDC Converters on the TPS65023 as follows:
Supply Voltage = 5V
------------------------------
DCDC1 = Should be 1.2V but is 2.0V
DCDC2 = 1.8V
DCDC3 = 3.3V
We're using…
Part Number: TPS65023 Hi TI,
I am supplying 3.3V into TPS65023.
If I want to set VDCDC1 as +1.5V, can it be done using external resistor divider on DEFDCDC1? Or must it be set using DEFCORE register via I2C interface?
thanks.
Part Number: TPS65023-Q1 Other Parts Discussed in Thread: TPS65023 , LM26480 Hi,
I was not able to find any PSRR data for the internal LDOs of the TPS65023.
Do you by chance have any data?
Thanks
Regards,
Alberto
Part Number: TPS65023-Q1 Other Parts Discussed in Thread: TPS65023 , TPS56C215 , TIDA-01480 , TPS62067 , , TPS568215 Hi Team,
Would you advise TI best match power solution for XAZU5EV FPGA?
I found TPS65023 is recommended for ZU5EV.
However I'm not sure…
Part Number: TPS65023 Other Parts Discussed in Thread: TPS6521815 Hi,
May I know if you have the driver code for TPS65023 when use with NXP CPU iMX6Solo/DualLite? We are looking for bootloader driver code.
Thanks.
Gim Song