Other Parts Discussed in Thread: TPS65023B We are using TPS65023B in one of our design with DM368.
There are two 1V comparators PWRFAIL and LOWBAT.
1) We do not need to use the comparators and would like to know how to terminate them.
I didn't find any…
Part Number: TPS65218D0 Other Parts Discussed in Thread: TPS65023B , TPS650250 Hi,
I have designed hardware for AM4376BZDND30S powered by its recommended PMIC TPS65218D0. PMIC TPS65218D0 is not available in the market, are there a drop in replacement for…
P. 36 of the datasheet seems to indicate that the default value of the DEFCORE register (06h) is 14h/1Eh (depending on the value of DEFDCDC1). This would mean a default core voltage of 1.3V/1.55V instead of 1.2V/1.6V as stated on p. 22.
Is p. 36 correct…
Hi Berkay,
TPS65218D0 and TPS65216 are the approved PMIC solution to power the AM437x processor. I would recommend getting the demand entered in the system so an ESD can be assigned.
We also have hardware configurable PMICs in our industrial portfolio…
Part Number: TPS65217 Other Parts Discussed in Thread: AM3354 , TPS65023B
Hi sir,
As you know, lots of ICs are out of stock.
The customer is looking for TPS65217CRSLR anxiously.
But it's out of stock, and the LT is very long.
I confirmed our catalog…
Other Parts Discussed in Thread: TPS65023B I am using the TPS65023B with a supercap for VBACKUP. I want VLDO1=1.8V and VLDO2=3.3V. I'm using VRTC to power VINLDO and I have the DEFLDO[2..1] pins tied to VRTC. This was working fine on the first cut…
Part Number: TPS650250 Other Parts Discussed in Thread: LMZM23601 , TPS65023B , Hi team,
My customer is working on a new battery input stage that will be used in several designs. For this development, the R&D team is looking for a low cost 24 Volt battery…
Other Parts Discussed in Thread: TPS65023B , TPS65023 , TLV320AIC3104 , AM3517 Hello.
I have a question about powering VDDS_DPLL_PER_CORE, VDDS_DPLL_MPU_USBHOST and VDDA1P8V_USBPHY, VDDA_DAC using LDO1 in TPS65023B powering on when 1.2V VDD_CORE comes up…
Hi Emily,
Thanks for your quick response.
We do have some further clarifications here as per the client's requirements:
The Primary issue is VDCDC3 being 3.3V when it is programmed to be 1.8V. Does the LDO programming affect the output voltage of…
Also, it should be noted that Variant 006 (for Artix-7) and Variant 007 (for Spartan-7) use the same building blocks (TPS62067, TPS568215, and TPS65023B) to power the FPGA. Note that TPS62067 can be replaced by TPS62097, but TPS62097 was not released…