Part Number: TPS650250 Other Parts Discussed in Thread: TMS320C6742 , TPS650061 , TMS320C6746 , TMS320C6748 Hi Team,
We are using TPS650250 to power C6746 DSP, however, as one DCDC is used to power Flash, when load becomes heavy, the output voltage will…
Part Number: TPS650250 Hi,
I am using TPS650250 in my design.
1. Can you please let me know how to calculate the power dissipation for PMIC.
2. What is the efficiency for DCDC1 for VI=5V and Vout=1V
3. What is the efficiency of DCDC3 for VI=5V and Vout…
Part Number: TPS650250 Hi Sir
The customer uses VINDCDC1 to input 5V and output 3.3V. When the EN pin is logic lowered, there is still output at 3.3V. May I ask why?
we change another IC in this board ,this phenomenon still excit .
tps650250 Schemetic and…
Part Number: TPS650250 Other Parts Discussed in Thread: TPS65023 Hi,
In my design Im not using PWRFAIL _SNS and PWRFAIL pins. Can i keep these unused pins open?
Part Number: TPS650250 Other Parts Discussed in Thread: TPS650231 Hi Team,
I am lookding for PMIC which satisfy below requirements:
Output:
1.2V-500mA MAX
1.8V-300mA MAX
2.5V-200mA MAX
2.8V-300mA MAX
3.3V-200mA MAX
Input:3.7V~5V;
Size: within 4*4m…
Part Number: TPS650250
Hi,
I am using TPS650250 to power my ARTIX-7 FPGA XC7A50T-2CPG236C.
Attached is the power tree used. And power estimation of ARTIX-7
As per xilinx datasheet minimum ramp time for all power rails should be 0.2ms. Can you please…
Part Number: TPS650250 Hello guys,
One of my customers is considering using TPS650250 for their new products.
They will use DCDC1 of the device for ARM CPU core as 1.26V power supply set by 2 external resisters (1.1k ohm - high side and 910ohm - low side…
Franco,
Thanks for the update. It might be helpful if you click the " Ask a related question " button and say your part number is AM3352 on the new thread.
If you mention the TPS650250 device I will still get notified, but the Sitara AM335x team…