Part Number: TPS650365-Q1 Tool/software: Hello All,
I can read TPS650365-Q1 registers through I2C but when tried to write on any register, The register doesn't update.
for example register 0x1d bit 0 doesn't change the value. So my question why can…
Part Number: TPS650365-Q1 When is the validation required for Following Assumption of Use? At evety power up cycle or at the EOL?
SA-16a: The system-integrator validates the TPS65036x(-Q1) functionality and TPS65036x(-Q1) Safety Mechanisms against System…
Part Number: TPS650365-Q1
Hi TI Engineer,
I am currently using I²C communication with the TPS65036x. I understand that register address 0x01 is the DEVICE ID register. I would like to ask whether all TPS65036x devices share the same ID…
Part Number: TPS650365-Q1 Other Parts Discussed in Thread: AWRL6844 I am currently designing a radar module using the TPS65036501RAYRQ1 PMIC in combination with the AWRL6844 radar sensor.
To proceed with the schematic design, I have searched for the…
Part Number: TPS650365-Q1 Tool/software: Hello,
In our project we shall use TPS65036X-Q1 as PMIC for our board.
For VLDO output capacitance min and max out capacitances are mentioned but system capacity is not mentioned. (For example 10uF capacitors…
Part Number: TPS650365-Q1 Tool/software: Due to PCB size limitation, it is not possible to accommodate an I2C interface. Is it feasible to use voltage divider resistor on FB_B1, FB_B2, and FB_B3 pins to adjust the output voltage?
Part Number: TPS650365-Q1 Other Parts Discussed in Thread: SN74AHCT1G08 Tool/software: Dear Supplier,
Kindly provide the weight information of the following part number:
1. AWR2E44P 2. TPS650365-Q1 3. AWRL6843DBSANCRQ1 4. SN74AHCT1G08 / TC4S11F…
Part Number: TPS650365-Q1 Tool/software: Hello Team,
I wanted to ask what kind of adapter is used for programming this device?
Is this adapter TI offers?
Does it have the same program adapter as the TPS650331?
Best regards,
My An
Part Number: TPS650362-Q1 Tool/software: Hi, All.
When I review the OPT sheet of TPS650365, I saw the Normal/Inverted Polarity.
That means active high and active low.
Normal Polarity is active high? (Inverted Polarity is active low)
Please…