Part Number: TPS650830 Other Parts Discussed in Thread: TPS22969 ,
Dear Support
The customer does not follow the EVM design, They change load switch TPS22969DNY (Q5&Q6) to other vendor item. The design is can't normal work, When SLP_SUS# is pulled high…
Part Number: TPS650830 Hi,
Do we have definition regarding timing requirement among any power rails or control signal from PMIC when the system has a transition from S0 to G3 mode? Or it's not reasonable to define this since it involved VIN<UVLO to trigger…
Part Number: TPS650830 Hi,
Based on the setting of FLT bits, we can long press PWRBTN to trigger an emergency shutdown. THe questions are,
After PWRBTNIN is released, how long it takes to finish an emergency shutdown?
Will all the register in UVLO domain…
Part Number: TPS650830 Hi Team,
In the TPS650830 data sheet, there are parts that seem to be wrong.
In the equation that determines the constant of overcurrent protection of equation (3) in P.131
Is not "x1.3" necessary?, Or "IOUTMAX" instead of "IOCL…
Part Number: TPS650830 Hi team,
Customer inquired that he could not get a low level out for RESETZ in low-out logic state.
The RESETZ pin is defined as a push-pull output in the datasheet.
He got a low signal level when pulling up with a resistor, such…
Part Number: TPS650830 Hi Experts,
While I was supporting one of our important customer, one important issue emerged. As the customer is using VR3 to generate a 3.3V output, which, has also been used as ENVR5 to enable VR5 when 3.3V ramps up. While I…
Part Number: TPS650830 Hello Team,
My customer is wondering if TPS650830 can support Coffee lake-S (35W)?
Can you share datasheet and DSN file to help them out with creating schematic?
Thanks a lot for help.
Martin
Part Number: TPS650830
Hi,
our customer is having two boards fail turning on 3.3V .
they had confirmed that the power of VREF1V25, LDO3, LDO5 and V3.3EN has correct output.
But VR3 doesn't have output.
May I have your comment for how to fix this…
Part Number: TPS650830 i was use TPS650830 in Kaby lake-Y platform,
now, Kaby lake-Y is upgrade to Kaby lake-Y Refresh,
Could you help check TPS650830 is also support Kaby lake-Y Refresh?
thanks!