Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS65131TPS65131RGE - Can a TI engineer please give us some clue as to why our -9V is ~0.8V? We've experimented with a number of values of R81 with no effect.
Adding layout if it offers any clues. We are completely stumped. Beyond…
Hi Matt,
I'll close this thread due to inactivity and if you have more questions, please reply to it directly and it will open again.
Please help to click "Resolve" if the problem is solved.
BR
Patrick
Part Number: TPS65131 Hi,
my customer is using TPS65131TRGERQ1 in an industrial application and due to supply situation is evaluating to use TPS65131RGER instead.
85degC is ok for the application, two open questions:
1. Electrical spec seem the same, therefore…
Part Number: TPS65131 I have also removed C118. Also, the chip is making a clicking noise.
I'm trying to get -9V and +9V out. Instead my +9V is 10.2V, my -9V is not stable, around -12 to -14 and always moving.
I have also removed R83 and R84 to…
Part Number: TPS65131-Q1 Other Parts Discussed in Thread: TPS65131 Hi team,
Can you recommend a AEC-Q100 solution for the following OLED spec?
-. ELVDD (4.6V) / ELVSS (-5V)
-. Current : 2.54A (typ.) / 2.92A (max.)
-. Power : 24.1W / 27.7W
Thanks,
…
Part Number: TPS65131-Q1 Hi,
Here is the datasheet for the part:
TPS65131-Q1 Positive- and Negative-Output DC-DC Converter datasheet (Rev. E)
On page 23, the datasheet shows several efficiency graphs. My application goes up to 80C. Typically, the efficiency…
Part Number: TPS65131 For our PCB we are using the TPS65131, however it does not work the way we expect it to.
As a starter our Vpos is at a steady 10V instead of 15V
And Vneg is either 0V or it jumps to -7 V and then slowly goes back to 0V and that jumps…
Part Number: TPS65131 Other Parts Discussed in Thread: LM5176 Hi
Please help suggest alternatives to LT8582
T he conditions are as follows
Current Mode FB
The output voltage VPOS 15~17V , VNEG1 -13~-11V
Thank you
Part Number: TPS65131 Other Parts Discussed in Thread: TPS65130 , Hi Team,
want to check if TPS65130 or TPS65131 can support +6V/>250mA, -6V/>250mA? Thanks.
BRs
Given
Part Number: TPS65131 Hi...
One of my customer is using TPS65131 for 5V input , +/-15V output configuration. They have an application where load current is very small (most of the time load will be 2mA & during relay drive +15V draws 200mA for 100mS…