Part Number: TPS65132 Tool/software: The footprint of the TPS65132W is not listed on the datasheet. There is a BGA version, but could you also include the WQFN version?
Part Number: TPS65132 Other Parts Discussed in Thread: TPS65131 Tool/software: Hi team,
Do TI have LCD bias solution for >6V Vpos, <-6V Vneg? Also, what does happen at TPS65132 when resistor divider is set to 6.1V or 6.2V @ Vpos?
Regards,
Hayas…
Part Number: TPS65132S Tool/software: Hi team,
Our customer tested this device and observed both of ±5V output voltage increase up to 0.8V when other IO supply (1.8V) start up in start up sequence when EN is Low.
The device condition is below,
Input…
Part Number: TPS65132 Tool/software: Hi team,
Customer comes to us check for AMOLED bias solution.
Vin = 5V;
Vout+ = 3.3V/200mA;
Vout- = -3.3V/200mA.
Could you help recommend suitable solution?
Thanks and Best Regards,
Will
Part Number: TPS65132 Tool/software: Hi team,
I am looking at the datasheet of TPS65132.
The function of the IC says that the inverting side will be made by boosting the input signal and inverting it.
How will the ic perform when Vout is larger…
Part Number: TPS65132 Hi
1.The TPS65132SYFFR chip uses a fixed output of ±5.4V and does not require I2C to adjust the voltage. Do the two I2C signal lines need to be processed? Can be left floating
2. D2 pin (AGND) is in the middle, with a 4mil line…
Part Number: TPS65132 Hello team,
My customer is in need of information on the UBM (Under Ball Metallization)/SRO (Solder Resist Opening) of this device TPS65132LYFFR.
They need this for their DFM team to define their own land pattern.
Thank…
Part Number: TPS65132 Hi team,
My customer ask if they could do I2C communication after enable bias voltage? and why the power sequence is different in different suffixes of TPS65132?