Part Number: TPS65149 page 24 of the datasheet says:
A Microsoft Excel spreadsheet is available that allows easy calculation of temperature compensation components and eliminates the need for the following expressions to be calculated manually. Contact…
Part Number: TPS65149 Hello,
On page 24 of the datasheet it says:
A Microsoft Excel spreadsheet is available that allows easy calculation of temperature compensation components and eliminates the need for the following expressions to be calculated…
Hello Kevin,
All versions of the TPS65175 does not include the discharge function. What are the requirements for this application ? Do you require all 12-Ch Level Shifter? Dependent on the criteria there is the
TPS65149 (8-Ch-L/s with discharge function…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.
Peter,
i am enclosing the Power Management Guide for 2011. The section you will be interested in starts on page 43 and actual devices listed on page 46, With the minimum information you have given me I would expect that you will want something like…
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…