Part Number: TPS65150 Hello,
We are using TPS65150 for LCD driver but we are not getting Vs boost output. We are getting 5V at Vs same as Vin.
Find attached Schematic
FET3562-C_V1.0_31122025.pdf
Part Number: TPS65150 Hi Team, We are using a 10.1" Display with the following voltage requirements -
As per the display driver datasheet , the current requirements for each of these voltages are - AVDD = 9.6V @ 10mA VGH = 18V @ 200uA VGL = -6V @…
Part Number: TPS65150 Tool/software: We are using the TPS65150PWPR IC to power our LCD. Below is the schematics along with the electrical parameters of the LCD module. We are encountering an issue where the input voltage appears on the output after the…
Part Number: TPS65150
Tool/software:
Hello, Please, I would like to know if the choosen component's values are correct considering my LCD needs. Below, there's a voltage need seen in the datasheet.
The schematic is shown below, where I've placed…
Part Number: TPS65150 Tool/software: Hi Team,
I'd like to request you the schematic design review. Please check the attachment below and let me know the review result.
Schematic_TPS65150 .pdf
Regards,
Part Number: TPS65150-Q1 The land pattern detail of the TPS65150QPWPRQ1 part is not available in the datasheet and we've already checked the ultra librarian. We require a specific land pattern that is not available in the ultra librarian. Could you please…
Part Number: TPS65150 Tool/software: As stated in a previous answer under the title 'TPS65150: Fault delay function question'...it is pointed out that the output rails need to be stabilised before FDLY delay ending or the chip may not function. But, for…
Part Number: TPS65150 Other Parts Discussed in Thread: TIGER Tool/software: Hi,
May I know when the REF pin will start to output?
Thanks and Best regards,
Tiger
Part Number: TPS65150 Tool/software: Hi,
I'm prototyping a design to power a 7" LCD using the TPS65150 IC.
Immediately after VIN rises to 3.3V, the IC enters the fault condition due to a Buck Overvoltage (If I disable the fault protection, the Boost…
Part Number: TPS65150 Tool/software: Could you check if below footprint picture is wrong! it should be 24pin, not 20pin! Please help to clarify it and update! Very thanks.