Part Number: TPS65185 Hi Team, I would like to configure the powerup sequence for my epdc panel, and the required sequence is VSS -> VDD -> VEE -> VNEG -> VPOS -> VDDH -> VCOM We've tried out the below sequence, Set WAKEUP pin HIGH and the PWRUP pin to…
Part Number: TPS65185 Hi, We are integrating an EPDC display with imx8 ulp, and require to configure tps65185 for the display. Is there a linux driver available for this PMIC?
Part Number: TPS65185 Tool/software: Previously, I mentioned in this thread that I was obtaining incorrect positive voltage values and that there were some noisy sounds in the circuitry:
https://e2e.ti.com/support/power-management-group/power-management…
Part Number: TPS65185 Dear TI Engineer,
Can you help confirm if the TPS651851 support EINK screens with a refresh rate of 80fps? If yes, how do we implement it?
Thanks,
Kind Regards
Part Number: TPS65185 We are currently developing an E-Ink tablet using the TPS651851RSLR as the PMIC.
During continuous operation, we observed that the PMIC occasionally shuts down automatically, and all power rails turn OFF.
After some minutes,…
Part Number: TPS65185 Tool/software: I have used reference design from https://vroland.github.io/epdiy-hardware/build/boards/epdiy-v7_schematic.pdf, my quistion is if i pull powerup and wakeup pin high without load all rail should on and shows output…
Part Number: TPS65185 Tool/software: Hello,
In TPS651851, can we increase the output voltage of Charge Pump-2 from 20V.
For Charge Pump 1- it can be increased to 28V according to datasheet page No 10.
Note: I need to increase the CP-2 voltage to…
Part Number: TPS65185 Tool/software: Hello TI engineers and people on board this awesome knowledge forum!
I'm Martin a hardware developer from Spain that helps in https://github.com/vroland/epdiy-hardware epdiy project that is an open source parallel…
Part Number: TPS65185 Tool/software: Hi Sarah,
I kindly request you to review the schematics of TPS651851 attached below and share your valuable comments.
Best Regards,
Monisha M
TPS651851_EPD_PMIC_08DEC2024.pdf
Part Number: TPS65185 Tool/software: I am designing a MIPI-DSI lcd board. There are AVDD, ELVDD and ELVSS power inputs and the required voltages are AVDD = 7V, ELVDD = 4.6V and ELVSS = -3.0V, I could use TPS65185 for my lcd power but i should seperate…