Part Number: TPS65216 Other Parts Discussed in Thread: AM3351 , Hi team,
My customer will use TPS65216 for powering AM3351.
VDD_CORE and VDD_MPU of AM3351 are same voltage so DCDC2 is unused. How to terminate FB2 and L2?
I referred the following E2E Jason…
Part Number: TPS65216 Other Parts Discussed in Thread: AM3356 , Hello,
we have a board with an AM3356 CPU that is powered by a TPS65216 PMIC.
We're use net console for U-Boot and want to detect an active ethernet link as fast as possible, ideally disabling…
Part Number: TPS65216 Other Parts Discussed in Thread: TPS65218D0 , TPS65218 We are trying to use the TPS65216DO to power the AMC335x. We are a bit confused on the RTC-only mode power connections. We are following the directions in the TPS65216 User Guide…
Part Number: TPS65216 We're facing a bug that is affecting leakage in power off.
For all these tests, PWR_EN is low and nWAKEUP is high, so the PMIC is off.
What we've found is that if AC_DET is pulled low, PGOOD is pulled low and the system remains…
Part Number: AM3358 Other Parts Discussed in Thread: TPS65216 Hi Expert,
PSDK can support AM335x and TPS65216?
Do I have to do any change for TPS65216 on SW?
Is there any reference design for AM335x and TPS65216?
Is there reference schematic or AM335x a…
Part Number: TPS65216 Other Parts Discussed in Thread: TPS6521815 Customer uses TPS65216 now and find a problem.
Customer changed DCDC2 register to 0xA4. RD thinks he has written it successfully because the read back value and the output voltage are able…
Part Number: TPS65216 Other Parts Discussed in Thread: TPS6521815 Hello,
All of the datasheet specification are centered around DCDC4 Vout = 3.3V. With 5Vin and 3.3Vout there is 1.6A maximum output current.
What is the maximum output current for 5Vin…
Part Number: TPS65216
I'm building a simple AM335x-based system using the TPS65216D0 powered from an external 5V source, but it's failing to power on.
I had planned on having the system power on immediately (since it's not a battery-operated…
Part Number: AM4372 Other Parts Discussed in Thread: TPS65216
Dear Champs,
My customer is bring-up AM4372 in their custom board and it was powered by PMIC(TPS65216). They found every power rails of TPS65216 were very unstable during several dozens of…
Part Number: TPS65216 Other Parts Discussed in Thread: BOOSTXL-TPS65218 , LP87524-Q1 Hi Team,
Customer is evaluating one PMIC from other vendor, general specs are as follow:
5 Regulator Rails for 4 Buck Converters and 1 LDO
CH1 : Buck, 0.6V to 1.39375V…