Part Number: TPS65217 Other Parts Discussed in Thread: AM3352 Hi team,
I am designing the TPS65217 for the AM3352 power supply.
According to AN(SLVA901), I'll use Rll on the BAT terminal to avoid brownout issue.
Rll is recommended to be 1k to 10k…
Part Number: TPS65217 Dear Expert
At present, TPS65217 power supply chip is used in the project, so the output voltage of VDD_MPU(DCDC2) needs to be set as 1.25V, and the default is 1.1V. It can be realized by the DCDC2 control register set in the specification…
Part Number: TPS65217 Hi,
I see the regulator address in tps65217.dts, and I have questions as below,
1. Why the address-cell and size-cell are <1> and <0> ?
2. Why the regulator address of dcdc1_reg is 0 ?
Thanks.
#address-cells = <1>;…
Part Number: TPS65217 Hello,
We are using the TPS65217 in one of our design, We have given the input power supply voltage of 5V to TPS65217 from an Isolated DC-DC module.
The input power to the isolated DC-DC module supplied by TPSM84209RKH - 5V.
TPS65217…
Part Number: TPS65217 Hello guys,
One of my customers is going to use TPS65217C for their new products.
At this moment, they have the following question. Could you please give me your reply?
Q. We don't use LDO2 output. According to TPS65217x Schematic…
Part Number: TPS65217 Using PMIC TPS65217CRSLR & we are facing SCM problem with this part. So do you have any suggested part which is having same parameters & one is to one replaceable ?
Please help.
SCM provide some alternate which are given…
Other Parts Discussed in Thread: TPS65217 Hi,
We have a board that look a like the beaglebone black.
But the TPS65217 is not available anymore.
I would like to get more direct information about whether substitutions or custom designs are possible for…
Part Number: TPS65217 Can I use the function of charging the external battery and using the external battery to power up other circuitry when not in charging mode.
Part Number: TPS65216 Other Parts Discussed in Thread: TPS65217 , , TPS65218D0 , TPS65219 The TPS65217 is listed as pin to pin with the TPS65216. Currently the TPS652162 is being used (For AM571x). Which version (OPN) of the TPS65217 would be the correct…