Part Number: TPS65217CEVM Hi,
This is K Harshavardhan.
We are working on TPS65217CEVM. All the module testing is almost done.
We got a battery of 3.7V and 850mAh to check the charge path.
But the battery is not charging with AC 5V and CHG_EN is high…
Part Number: TPS65217CEVM Other Parts Discussed in Thread: TPS65217 HI,
This is Harshavardhan and we have ordered a PMIC EVM (TPS65217C).
We are trying to validate the PMIC.
Do we have any provision of giving the separate input (apart of AC or battery…
Part Number: TPS65217CEVM Other Parts Discussed in Thread: LM5576 In the datasheet, the PB_IN pin is connected to 5V internally and can be connected to GND externally with LOW level enabling. However, when I use TPS65217C, some TPS65217C can work with PB_IN…
Part Number: TPS65217CEVM Other Parts Discussed in Thread: TPS65217 Hi
This is K Harshavardhan.
1. I kindly request you to provide the basic parameters has to be checked/ Tested in TPS65217CEVM.
2. What are the functional test required in EVM.
3. GIve…
Part Number: TPS65217CEVM Other Parts Discussed in Thread: TPS65217 , Tool/software: Linux I would like the default values for your Power Management tps65217C arbitrarily pretend! Is that possible ?
I have a Beaglebone Black and this one has in status…
Part Number: TPS65217CEVM Hi all,
In one our product we are using tps65217c pmic for powering am335x processor. this devices we are selling for last 3 years , but from last few months we are getting problem of getting pmic and processor failure problem…
Part Number: TPS65217CEVM Other Parts Discussed in Thread: TPS65217 Hi all,
In one of our design TPS65217c is used to power AM335X processor. And PMIC does not generating Sys_voltage. SYS_VOLT level is 2.4V.
we are getting POWER_EN High for 50mS and then…
Other Parts Discussed in Thread: TPS65217 Yes but in Sleep Mode the Device do not Charge my Battery but that is that what i want .... And the I2C is OFF so i cant say to the Modul Charge my Battery ! SO i HAVE to Modify my Driver but how can i do that…
Hi Brenda,
here the answers:
1. Which EVM did they order? TPS65217CEVM or TPS65217DEVM ?
TPS65217CEVM
2. Are they using the USB2ANY or they are supplying the 3.3V with an external supply?
Supply 3.3V externally
3. Does the customer have the default…
Hi Cindy,
The figure below shows the recommended connections for the power path. This information can be found in the Brownout report.
Here I'm listing some links with more information in addition to the datasheet which can be used as a reference when…