Part Number: TPS65218
Dears,
Good day!
TPS65218B1RSLT and TPS65218B1RSLR are NRND. Are they EOL soon?
Would you please help to advise their replacement? Thanks.
Hi Ishiwata,
That is odd that the customer's USB2ANY does not show the expected 3.3V supply at JP4 pin "V3p3". Please have the customer use our USB2ANY Explorer software to verify the USB2ANY is the correct firmware version and recognized…
Part Number: TPS65218D0 Other Parts Discussed in Thread: TPS65218 , Hi Team,
Can TPS65218D0 directly replace tps65218? What are the main differences between the two? Thanks.
Regards, Charlie
Part Number: TPS65218 Hi
I have the following questions about TPS65218.
1. Can you recommend the Coin cell specification that connects to CC pin? (ex. 3.7V/ ?Ah)
2. I won't use DCDC5. How do I connect the pins?(open or connection gnd ?)
Thanks
Part Number: TPS65218 Hi team,
Could you give me comment on following customer question?
Q1. What is the default value on CONFIG1?
The customer verified the default value on CONFIG1 after powering on the device, but they could read 0x48, not 0x4C as expected…
Part Number: TPS65218
In the datasheet. At light load currents the converter operates in power save mode. customer would like to know whats the limit of light load current. When in which current, device will enter power save mode
Part Number: TPS65218 Other Parts Discussed in Thread: IPG-UI , , , USB2ANY Hi Brenda,
I've just downloaded IPG-UI and in when go to "Select Device" I do not have the TPS65218-1.2 in the drop-down menu. As I result that I have only TPS65218-1.1,…
Part Number: TPS65218 Other Parts Discussed in Thread: AM4378 Hi team,
Here is one question about the resistor value on TPS65218 CC pin.
On both our datasheet and EVM, a 10Ohms resistor is connected on the CC pin.
But on our AM4378 EVM, we are using…