Part Number: TPS6521815 Other Parts Discussed in Thread: TPS53631 Tool/software: Dear Team,
Do you have Intelli-PhaseTM Solution parts that can replace MP87440 and MP87420?
A cross-reference search couldn't yield any part numbers.
BR,
Part Number: TPS6521815 Tool/software: Hi team,
Customer would check, do we get PMIC could generate following power rail for uOLED screen?
Vin = 3~5V
Thanks and best regards,
Will
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218 , USB2ANY , IPG-UI Tool/software: Hi team,
Our customer is considering installing a blank TPS65218 and then programming it on-board. If VIN_BIAS is set to 5V and USB2ANY is connected via I2C…
Part Number: TPS6521815 Hi Team,
As we are using TPS6521815 PMIC for powering Cyclone V FPGA. So, we are planning to do power Integrity analysis for that we need an information from your side.
What is the ROUT and LOUT of the Pin L1, L2, L3, DCDC4, LDO1…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218D0 , TPS51206 , TPS65218 , TPS51200 Hello,
Hope you are doing well,
We are using TPS6521815 PMIC for powering Cyclone V GX with DDR3 memory, having few queries with sequencing and configuration…
Part Number: TPS6521815
Hi, I search for PMIC for Vatics SiP module I5S series.
The Vatics part number is I5502S.
Inpu t voltage of desired PMIC is 4.9-5.1V
Outputs of desired PMIC are total number of 5: 1.05V/1.8A max 1.2V/1.8A max 1.8V/1.8A max 3.3V/2A ma…
Part Number: TPS6521815 Hi,
I have a question about "Note" in datasheet P45, 8.5.1 Programming Power-Up Default Values.
<Note>Only bits marked with (E2) in the register map have EEPROM programmable power-up default settings. All other bits keep…
Part Number: TPS6521815 Hi, I'm Taka.
I use the PWR_EN pin for power up.
The PWR_EN pin has a deglitch circuit and the deglitch time is typ 10ms.
What is the maximum and minimum deglitch time?
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218 , TPS6521855 Hi Brenda,
It is about PMIC TPS6521815 In system Programming.
The MAIN question is: Is it possible to program/re-program the TPS6521815 with PWR_EN set LOW?
For our design…